SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
During the provisioning process, the SimpleLink device might automatically restart itself as part of the process. If a restart is required while the host application is busy (for example, when the host has opened sockets during external configuration provisioning), instead of performing the restart automatically, the networking subsystem asks the host application to do it. When this event arrives, the host should stop its activities (for example, close all opened sockets), and restart the device by issuing sl_Stop and sl_Start commands.