SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
DELETE requests are handled in a similar way to POST requests. The only difference (aside from the command type received) is that there is no processing of RESTful APIs; all requests are transferred directly to the host. As in POST, the response cannot contain any payload, only HTTP headers.