SWRU473A February 2017 – August 2018 CC3120MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF
The application includes the following tabs: Provisioning, Devices, and Settings. Additional LAN and OTA tabs are applicable to the OOB only, and are automatically opened after provisioning is successfully completed. If these tabs do not appear, navigate to the Devices tab and select the device by pressing and holding it.
If the device has never been provisioned, follow the Section 6.1.1. If the device has already been provisioned, it automatically connects to an AP, so users can start playing with LAN and OTA demonstrations. If the AP credentials have not been provisioned by the user’s SimpleLink Wi-Fi Starter Pro application, or if the SimpleLink Wi-Fi Starter Pro application has been started while the device is already provisioned and connected to the AP, it is required to bind the application to the desired device. Users would need to navigate to the Devices tab and select the device by pressing and holding it.