TIDUEJ6A January 2019 – July 2022
In the implementation discussed in this reference design, the MSP430FR6043 MCU performs the complete acquisition process using the USS module in the device for signal conditioning. Figure 3-3 shows this acquisition process.
At the beginning of the sequence, the MSP430FR6043 MCU sends a train of pulses to the first transducer, XDCR1. The signal is then received by the second transceiver, XDCR2 , after propagation time T12. The difference in time between transmission and reception determines the upstream (UPS) ToF, or ToFUPS .
The MSP430FR6043 MCU repeats the same process in the opposite direction during the downstream stage, resulting in the propagation time, T21, which represents the downstream (DNS) ToF, or ToFDNS.
The DToF, Δt, can then be calculated as the difference between T12 and T21, as described in Equation 3.
The DToF is typically measured using two techniques: Zero-crossing using a time-to-digital converter (TDC) or through Correlation using the ADC captured signal
The TIDM-02003 design uses the ADC-based technique instead of the TDC technique due to the following advantages.