TIDUF52 December 2023 MSPM0L1303 , MSPM0L1304 , MSPM0L1305 , MSPM0L1306 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
This design adopted a modulation-based smoke sensing signal chain to overcome the limitations of the DC-based signal chain. As shown in Figure 2-4, the smoke signal is modulated to frequency fmod by sending a series of LED pulses at the frequency of fmod. The frequency, fmod, is selected to be far from the frequency of different types of ambient lights; for example, the LED and incandescent light interference located around 120 Hz along with harmonics of the 120-Hz fundamental frequency, and florescent light interference located around 44 kHz along with harmonics of the 44-kHz fundamental frequency. The modulated signal with ambient light interference is filtered by a bandpass filter with a center frequency located at fmod. The interference is attenuated by the bandpass filter while the smoke signal is retained. The signal is then demodulated back into baseband while the low-frequency interference is modulated up to fmod. With additional low-pass filtering, the interference is attenuated again, yielding an interference-free smoke signal around DC at the baseband. The demodulated signal is sampled by an Analog-to-Digital Converter (ADC) and stored for further post-processing. The modulation, demodulation, filtering and sampling is operated pulse by pulse. Better SNR can be achieved by sending a higher number of pulses (stronger filtering, more averaging, and lower noise) at the cost of power consumption.