TIDUF52 December 2023 MSPM0L1303 , MSPM0L1304 , MSPM0L1305 , MSPM0L1306 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
This section shows the plots of the transient recordings from the UL Fire Room tests for both the SASI smoke detection module and the optical obscuration reference meter. These plots demonstrate the successful smoke detection against various smoke types as well as the no false alarm result from the cooking nuisance source.
The raw response from the Blue and IR LED measurements are presented as a current transfer ratio (CTR). This measurement is the received photodiode current divided by the corresponding LED current. The ratio of the Blue and IR responses is also plotted to illustrate the usefulness to help distinguish various fire types. The reference measurement for the smoke data is captured by the reference meter and is given in units of obscuration rate (% / foot).
Figure 3-20 shows the transient plot of the Go-No-Go Flaming Polyurethane test, which includes both the Cooking Nuisance source (beginning of test up to 1.5 %/ft obscuration) and the Flaming Polyurethane source (ignited as the cooking nuisance source is turned off at the 1.5%/ft time). Figure 3-21 shows the transient plot for the Wood Fire test. Figure 3-22 shows the transient plot for the Paper Fire test. Figure 3-23 shows the transient plot for the Smoldering Smoke test. Figure 3-24 shows the transient plot for the Smoldering Polyurethane test.