TIDUF52 December 2023 MSPM0L1303 , MSPM0L1304 , MSPM0L1305 , MSPM0L1306 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346
Figure 2-12 shows the schematic of the LED drive. The transistors are controlled by the modulation signals LED_BL_MOD and LED_IR_MOD to turn the LEDs on and off. The limiting resistors R_BL and R_IR are designed to have nominal LED current as:
The IR and BLUE LEDs are selected as TSAL6100 and C503B-BAN, respectively. The typical forward voltage, VF, in the respective data sheets is used in Equation 9 to calculate nominal LED current. The supply voltage, VDD,LED is a regulated output of 5 V, derived from the battery by TPS7A2405, which helps maintain a consistent LED current and smoke sensitivity consequently. If a different LED current is desired, the current-limiting resistors can be replaced accordingly.
As the LED current is not regulated from a constant current source, the output power from the blue and IR LEDs varies across temperature. This results in a signal chain gain variation across temperature. This variation can be addressed by temperature compensation in digital post-processing of the signal chain output by monitoring the ambient temperature using either or both of the onboard temperature sensors of the M0L MCU and the HDC2010.