TIDUF72 August 2024
There are two configurations for the TIDA-010944 block diagram: either one- or single-phase (Phase A and Neutral, 1P2W, Wye) or split-phase (Phase A to Phase B, 2P2W, Delta) configuration.
In the split-phase configuration, the voltage is measured between Phase A and Phase B, which are 180 degrees apart.
In the single-phase configuration the Phase (or line) A line-to-neutral voltage is directly measured, as well as the two currents on Phase A and Neutral. The non-isolated ADS131M02 standalone ADC is used to measure both current and voltage on Phase A, while the AMC131M03 only measures the current through Neutral.
A separate shunt sensor is used on each of the 2 phases for the current measurement while a simple voltage divider is used for dividing down the corresponding voltage between Phase A and Neutral or Phase A and Phase B. The selection of the shunt is made based on the current range required for the energy measurements, with common values being in the range of 150μΩ to 200μΩ, assuming that a maximum current per phase of 60A–120A has to be measured.
In this design, the one AMC131M03 and one ADS131M02 devices interact with the MSPM0+ MCU in the following manner: