RTDs, or resistance temperature detectors, are sensors used to measure temperature. These sensors are the among the most accurate temperature sensors available, covering large temperature ranges. However, getting accurate measurements with precision analog-to-digital converters (ADCs) requires attention to detail in design of measurement circuits and calculation of the measurement. This application note starts with an overview of the RTD, discussing their specifications, construction, and details in their use in temperature measurement. Different circuit topologies with precision ADCs are presented for different RTD configurations. Each circuit is shown with a basic design guide, showing calculations necessary to determine the ADC settings, limit measurement errors, and verify that the design fits in the operating range of the ADC.
RTDs are resistive elements that change resistance over temperature. Because the change in resistance is well characterized, they are used to make precision temperature measurements, with capability of making measurements with accuracies of well under 0.1°C. RTDs are typically constructed from a length of wire wrapped around a ceramic or glass core. RTDs may also be constructed from thick film resistors plated onto a substrate. The wire or resistance is typically platinum but may also be made from nickel or copper. The PT100 is a common RTD constructed from platinum with a resistance of 100 Ω at 0°C. RTD elements are also available with 0°C resistances of 200, 500, 1000, and 2000 Ω.
The relationship between platinum RTD resistance and temperature is described by the Callendar-Van Dusen (CVD) equation. Equation 1 shows the resistance for temperatures below 0°C and Equation 2 shows the resistance for temperatures above 0°C for a PT100 RTD.
The coefficients in the Callendar-Van Dusen equations are defined by the IEC-60751 standard. R0 is the resistance of the RTD at 0°C. For a PT100 RTD, R0 is 100 Ω. For IEC 60751 standard PT100 RTDs, the coefficients are:
The change in resistance of a PT100 RTD from –200°C to 850°C is displayed in Figure 1-1.
While the change in RTD resistance is fairly linear over small temperature ranges, Figure 1-2 displays the resulting non-linearity if an end-point fit is made to the curve shown in Figure 1-1.
The results show a non-linearity greater than 16 Ω, making a linear approximation difficult over even small ranges. For temperatures greater than 0°C, temperatures can be determined by solving the quadratic from Equation 2. For temperatures lower than 0°C, the third order polynomial of Equation 1 may be difficult to calculate. Using simple microcontrollers, determining the temperature may be computationally difficult and using a look-up table to determine the temperature is common practice.
Newer calibration standards allow for more calculation accuracy using higher order polynomials over segmented temperature ranges, but the Callendar-Van Dusen equation remains a commonly used conversion standard.
RTDs have good interchangeability. This means that there is little variation from sensor to sensor because of good accuracy tolerance. This allows for good measurement accuracy, even if RTD sensors are replaced from system to system.
There are two tolerance standards that define a grade or class for platinum RTD accuracy. The American standard is ASTM E1137 and is used mostly in North America. The European standard is known as the DIN or IEC standard. DIN IEC 60751 is used world wide. Both standards define the accuracy of the RTD starting with a base resistance of 100 Ω at a temperature of 0°C.
Table 1-1 shows the specifications of different classes of RTDs. In both standards, the RTD has the tightest tolerance at 0°C. An absolute error is combined with a proportional error that has a temperature coefficient.
TOLERANCE | TOLERANCE VALUES (°C) | RESISTANCE AT 0°C (Ω) | ERROR AT 100°C (°C) |
---|---|---|---|
ASTM Grade B | ± (0.25 + 0.0042 • |T|) | 100 ± 0.1 | ± 0.67 |
ASTM Grade A | ± (0.13 + 0.0017 • |T|) | 100 ± 0.05 | ± 0.3 |
IEC Class C | ± (0.6 + 0.01 • |T|) | 100 ± 0.24 | ± 1.6 |
IEC Class B | ± (0.3 + 0.005 • |T|) | 100 ± 0.12 | ± 0.8 |
IEC Class A | ± (0.15 + 0.002 • |T|) | 100 ± 0.06 | ± 0.35 |
IEC Class AA | ± (0.1 + 0.0017 • |T|) | 100 ± 0.04 | ± 0.27 |
1/10 DIN(1) | ± (0.03 + 0.0005 • |T|) | 100 ± 0.012 | ± 0.08 |
The specified temperature range of each RTD class tolerance becomes smaller with more accurate grades and classes. Additionally, the range varies with the RTD construction type. For more details about tolerance values and temperature ranges, consult the data sheets of the RTD manufacturer.