SBAA457 June 2021 PCM6240-Q1 , PCM6260-Q1 , PCM6340-Q1 , PCM6360-Q1
All trademarks are the property of their respective owners.
TI is transitioning to use more inclusive terminology. Some language may be different than what you would expect to see for certain technology areas.
The PCM6xx0 device family includes the following high-performance, analog-to-digital converters (ADC):
This family of devices features a flexible audio serial interface that allows the device to be configured as either a controller or target. This document describes the modes, input parameters, and register coefficients required to configure the PCM6xx0 devices as an audio bus controller.