Applications such as Hot-swap where Power FET is operated in saturation region under high stress, FET safe operating area (SOA) is a major concern for system designers. Designers need to study the FET SOA curve available in the manufacturers data sheet and determine if the FET can handle the power stress without undergoing damage. This application report covers the significance of FET SOA, how the manufacturers derive SOA plot, and how the hot-swaps designers make sure that external FET is operated within specified SOA. Then, the eFuse protection schemes which help to ensure SOA of the integrated FET are discussed and a detailed method of deriving AOA (Allowed Operating Area) plot from the eFuse data sheet is presented. Finally, design recommendations are shared to prevent violation of eFuse abs maximum rating, and to provide long term reliability of eFuse.
All trademarks are the property of their respective owners.
SOA defines the maximum value of VDS, IDS, and time envelope of operation which the device can be expected to operate without getting damaged.
The entire SOA is made up of five distinct limitations, each of which shape the overall curve, as shown in Figure 1-1, the SOA for TI’s 100 V D2PAK CSD19536KTT.
Four of these limitations can be easily calculated from the known FET parameters – the RDS(ON) limit, the current limit, the maximum power limit, and the BVDSS limit.
The fifth and the most critical region is the thermal instability region, which cannot be determined with formulas, but must be tested. This portion of the SOA, noted by where the curve deviates from the constant power line that necessarily has a slope of -1 on a current vs. voltage log-log scale, indicates where thermal runaway can occur. The steeper the slope, the more prone the FET is to enter into thermal runaway condition at higher operating voltages. This region can also be called electro-thermal SOA as explained in Section 3. To plot thermal instability region there are two methods:
After having looked in detail about FET SOA , here are some FET failure modes that can occur on violating SOA.
Overall, it can be shown that the violation of maximum junction temperature specification of FET causes the FET to fail. Ensuring FET junction temperature is always at a safe level, also helps in ensuring that FET operates in SOA.