SPRUIY3 February 2023 TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1
This migration guide describes the hardware and software differences to be aware of when moving between F28002x, F280015x and F280013x C2000™ MCUs. This document shows the block diagram between the three MCUs as a visual representation of which blocks are similar or different. It also highlights the features that are unique between the three devices for all available packages in a device comparison table. A PCB hardware section has been added to aid in migration between packages that are in common between the devices. All three devices have the 64-pin PM and 48-pin PT/PHP packages in common. F28002x and F280015x have an additional 80-pin PN package in common, and F280013x and F280015x have an additional 32-pin RHB package in common. The digital general-purpose input/output (GPIO) and analog multiplex comparison tables show pin functionality between the three MCUs. This is a good reference for hardware design and signal routing when considering a move between the three devices. Lastly, like the F28002x device, the F280015x and F280013x software support is only in EABI format.
C2000™ is a trademark of Texas Instruments.
All trademarks are the property of their respective owners.
F280015x and F280013x are a subset of F28002x. The three devices have two packages in common: 48-pin and 64-pin. F28002x and F280015x have an additional 80-pin package in common. F280015x and F280013x have an additional 32-pin package in common. It is possible to migrate between F280013x, F280015x and F28002x with the caveats in this document taken into account.
An overlaid block diagram of F28002x, F280015x and F280013x is shown in Figure 1-1 while feature comparison of the superset part numbers for the F28002x, F280015x and F280013x devices is shown in Table 1-1.