SPRUJ60A April 2024 – October 2024 TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SJ-Q1
This migration guide describes the hardware and software differences to be aware of when moving between F280013x/15x and F28P55x C2000™ real-time MCUs. This document shows the block diagram between the two MCUs as a visual representation on what blocks are similar or different. It also highlights the features that are unique between the two devices for all available packages in a device comparison table. The F280013x and F28P55x devices have one package in common 64-pin PM. The F280015x and F28P55x devices have two packages in common; 80-pin PN and 64-pin PM so a PCB hardware section has been added to aid in migration between the three common packages. The digital general-purpose input/output (GPIO) and analog multiplex comparison tables show pin functionality between the two MCUs. This is a good reference for hardware design and signal routing when considering a move between the two devices. Lastly, like the F280013x/15x device, the F28P55x software support is only in EABI format.
C2000™ is a trademark of Texas Instruments.
All trademarks are the property of their respective owners.