Sarah Anthraper
The robotics market continues to grow as manufacturing becomes more automated and consumers implement these systems into their homes. Companies are beginning to automate manufacturing systems into their factories and warehouses, and adjust to a future where robots interact more with humans.
Design engineers who create robots understand there are hundreds of different types of robotics systems. As shown in Figure 1, robots range from small, helpful cobots that operate with a few watts of power to autonomous mobile robots to humanoid robots to heavy-duty industrial robots that operate up to 4kW and greater.
Robot manufacturers encounter several design challenges when developing advanced systems. The above robotics applications typically use 48V rail and support payloads from 2kg to 40kg. Engineers designing for higher loads must consider both mechanical and design implications to accommodate higher power levels. Higher currents can result in poor system performance caused by electromagnetic interference (EMI) or high switching losses. Functional safety is also a big factor, since robots are often used in environments with humans. Designing systems that will safely shut down when necessary is extremely important, whether it’s on a manufacturing floor or in a consumer’s home.
Smart single half-bridge gate drivers such as TI’s DRV8162 give you the flexibility to create integrated systems that can withstand large power and voltage ranges while reducing EMI and complying with functional safety standards.
Our smart gate drivers feature TI’s IDRIVE adjustable gate drive current scheme to control MOSFET slew rates across multiple levels of gate current. The DRV8162 has 16 adjustable granular settings as shown in Figure 2 to control when selecting your MOSFET and end application. For more details about IDRIVE, read Understanding Smart Gate Drive.
Using Equation 1, you can estimate what IDRIVE setting would be best for your system using the gate-drain charge (Qgd) specification of your MOSFET and the rise and fall time of the MOSFET’s maximum voltage between drain and source. These values vary depending on your system performance requirements.
If the IDRIVE is not close to a gate drive setting in the device you’re using, you will need additional passive components (including gate resistors) to achieve the required gate current. These additional components add to the overall bill-of-materials cost and contribute to added size in the printed circuit board (PCB), which can be worrisome for smaller designs in cobots, mobile robots and humanoid joints.
An external gate resistor is necessary when using competing half-bridge gate drivers, since they only provide a fixed current or two to four discrete settings. The 16 gate-drive settings in the DRV8162 driver and programmable source and sink ratio give you the flexibility to remove external passive components and simplify your design.
The wide Qgd support allows you to use the driver across various low-, mid- and high-power robotics platforms with different MOSFETs without having to change the gate driver design in each system. The source and sink gate currents for DRV8162 can be set as low as 16mA and 32mA respectively, and up to 1024mA and 2048mA. For example, a 1V/ns slew rate in a 48V system can be used to calculate a 48ns Trise/Tfall. This results in a range of 0.77nc/1.54nC to 49.15nC/98.30nC MOSFET Qgd that the device can support.
The DRV8162’s single half-bridge architecture enables placement closer to the FETs than a three-phase integrated gate driver. Figure 3 shows two circular PCB designs comparing a three-phase to a single-phase half-bridge implementation.
Placing the gate driver closer to the FETs reduces the length of traces, improves signal integrity, and reduces parasitics on the gate and source nodes. Shorter paths also help lower the effects of trace inductance, resulting in lower ringing and lower EMI.
In addition, DRV8162 helps improve system efficiency and acoustics with a 20ns dead time, which also helps enhance the operating pulse-width modulation duty-cycle range and thus the speed range, while increasing the available voltage to the motor. A lower dead time also minimizes diode conduction losses, improving system efficiency, and reduces motor current distortion and thus lowers audible noise. These effects improve overall performance and efficiency of the system.
Many robots operate alongside humans, so it’s critical to shut down the system in case of a power failing power source, power surge or short-circuit. A failure to a motor-drive application where the torque of the device is unpredictable could result in a dangerous situation. Because some machinery operates in industrial environments that involve heavy loads, it is important to be able to safely shut down, as well as prevent unexpected startup.
The International Electrotechnical Commission (IEC) 61800-5-2 standard defines a safety function called safe torque off (STO) in circuit design, which prevents power to the motor. The DRV8162 and TI’s DRV8162L incorporate a split-supply architecture to help you implement STO in your system.
In higher-power designs, engineers can refer to the 48V, 4kW Small Form-Factor Three-Phase Inverter Reference Design for Integrated Motor Drives (TIDA-010956), which features the DRV8162L with a 48VDC input and 85ARMS output current. As shown in Figure 4, this design includes a proposed STO concept, parallel FETs, high power and a single half-bridge gate driver.
Existing motor designs for robots use discrete implementation to meet safety requirements, which increases the board size and bill of materials. Smaller, safer and integrated gate drivers such as the DRV8162 are needed to improve efficiency and safety in robots of all shapes and sizes. New smart single half-bridge gate drivers help designers scale power from 10W to 4kW and greater, while shrinking PCB size, improving performance and safety – and delivering the flexibility to accelerate robot innovation for many years to come.
All trademarks are the property of their respective owners.
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2024, Texas Instruments Incorporated