>> TI Home > DSP Village > DSP University > DSP Educators' Information Exchange >

Resources  DSP University Educators Information ExchangeGray Rule

> Type of Materials
> Application Area
> DSP Family
> Type/Level of Lab
> Major Emphasis of Course
   > Theory
   > Lab
   > Application
  
Theory

Name/Title of Material: TMS320C3x DSP Teaching Kit
Author: Mehmet Akhan/Keith Larson
University: University of Hertfordshire/Texas Instruments
Email: dsph@ti.com
DSP Platform on which Material is Based: TMS320C3x
DSP Device on which this Material is Based: TMS320C3x
DSP Development Tools Used in Material: TMS320C3x DSK
Type of Material: Lecture Materials, Lab Exercises
Application Area: None
Type/Level of Lab: Introductory Undergraduate
Is the Lab a Primary Focus of the Course?: No
Major Emphasis of Course for which Material was Developed: Theory
Language in which Material is Written: English
Developed/Last Updated Date: August 1998
Computer Language in which Material is Written: Assembly, C
File Types: Word, PowerPoint, Executable/Source Code
Files: TMS320C3x DTK.zip (13.6M)
Description/Value to Others: These materials are lecture slides with accompanying instructor and student notes, suggested test questions, and five demo programs previously offered by TI as the TMS320C3x DSP Teaching Kit. They cover five lectures on DSP theory and demonstrate the software and basic capabilities of the C3x DSK board. The demos cover number representation, the speed of the floating-point multiply and accumulate operation, tone generation, analog to digital conversion, use of an FIR filter, how analog signals appear in the frequency domain, and an introduction to developing a DSP system taking into account communication between the DSP and digital to analog converter and sine wave generation.


Name/Title of Material: TMS320C5x DSP Teaching Kit
Author: Mehmet Akhan/Keith Larson
University: University of Hertfordshire/Texas Instruments
Email: dsph@ti.com
DSP Platform on which Material is Based: Other (TMS320C5x)
DSP Device on which this Material is Based: TMS320C5x
DSP Development Tools Used in Material: TMS320C5x DSK
Type of Material: Lecture Materials, Lab Exercises
Application Area: None
Type/Level of Lab: Introductory Undergraduate
Is the Lab a Primary Focus of the Course?: No
Major Emphasis of Course for which Material was Developed: Theory
Language in which Material is Written: English
Developed/Last Updated Date: 4/97
Computer Language in which Material is Written: Assembly, C
File Types: Word, PowerPoint, Executable/Source Code
Files: TMS320C5x DTK.zip (3.3 Mb)
Description/Value to Others: These materials are lecture slides with accompanying instructor and student notes, suggested test questions, and five demo programs previously offered by TI as the TMS320C5x DSP Teaching Kit. They cover five lectures on DSP theory and demonstrate the software and basic capabilities of the C5x DSK board. The demos cover playing a musical tune, the speed of the multiply and accumulate operation, quantization errors, aliasing, a low-pass filter, displaying graphical displays of the signals using the software tools, and an introduction to developing a DSP system taking into account communication between the DSP and digital to analog converter and sine wave generation.


Name/Title of Material: C5000 DSP Teaching Kit
Author: Mehmet Akhan/Keith Larson/Richard Sikora/Walter J. Gomes III
University: University of Hertfordshire/Texas Instruments/iDSP
Email: dsph@ti.com
DSP Platform on which Material is Based: TMS320C5000
DSP Device on which this Material is Based: TMS320C54x
DSP Development Tools Used in Material: TMS320C5402 DSK
Type of Material: Lectures, Tutorials, Lab Exercises
Application Area: None
Type/Level of Lab: Introductory Undergraduate
Is the Lab a Primary Focus of the Course?: No
Major Emphasis of Course for which Material was Developed: Theory
Language in which Material is Written: English
Developed/Last Updated Date: March 2001
Computer Language in which Material is Written: Assembly, C
File Types: Word, PowerPoint, Executable/Source Code
Files: TMS320C5000 DTK.zip (17.9 M)
Description/Value to Others: These materials are lecture slides, instructor notes, suggested test questions, and 5402 DSK-based programs previously offered by TI as the TMS320C5000 DSP Teaching Kit. Included are:

  • Six chapters of information on DSP and C5000 DSP architecture including slides, lecture notes, and test questions for each chapter.
    • Chapter 1: Introduction to DSP (includes C5000 architecture overview)
    • Chapter 2: From Analog to Digital
    • Chapter 3: Filtering
    • Chapter 4: The Frequency Domain
    • Chapter 5: Applications of DSP
    • Chapter 6: Assembly Language Basics
  • Fourteen C5000 DSP assembly language tutorials
  • Five demo programs that demonstrate the Code Composer Studio software and as well as the capabilities of the C5402 DSK board. The demos cover number representation, the speed of the fixed-point multiply and accumulate operation, analog to digital conversion, how analog signals appear in the frequency domain, and digital filters.
All files are editable so instructors can customize the materials.