> Type of Materials
> Application Area
> DSP Family
> Type/Level of Lab
> General EE
> Non-EE
> Introductory undergraduate
> Advanced undergraduate
> Introductory graduate
> Advanced graduate
> TMS320C6000
> TMS320C5000
> TMS320C2000
> TMS320C3x
> Other DSP Platform
> Other
> Major Emphasis of Course
|
|
Advanced Graduate
Name/Title of Material: DSP systems design
Author: Evangelos Zigouris
University: University of Patras
E-mail: ez@physics.upatras.gr
DSP device on which material is based: TMS320C6000
DSP development tools used in material: TMS320C6211 DSK
Type of Materials: Lab Exercises
Application area: Communications, General Signal Processing
Type/level of lab: Advanced graduate
Is the Lab a primary focus of the course? Yes
Type of course for which material was developed: Lab
Language in which material is written: English
Developed/Last Updated Date: 28/03/02
File types: Archived Source, Adobe Acrobat PDF
File: DSP System Design.zip (3M)
Computer Language on which the material is based: C
Description of item(s)/value to others: The DSPlab_programs.zip file contains the programs of the laboratory that takes place in the Master course in Electronics, at the Department of Physics, in Patras, Greece. In the DSPlab.pdf the programs and some theory of the applications are described. Finally, the submitted paper to the DSP2002 conference,3-5 July Santorini, Greece, which is based in this real-time DSP course, is in the DSP2002_paper.pdf
|