TLK100SAMPLE-CODE
TLK100 サンプル・コード
TLK100SAMPLE-CODE
概要
Purpose:
Sample C code is meant to give an example of the proper way to operate the various functions and capabilities of the PHY.
Overview:
The code was written in C using Microsoft Visual Studio 6.0 IDE. Debugging was done by interfacing Spirent SmartBits®-200/2000 (SMB- 200/2000).
Structure:
- The code is built of several C and header files.
- The resource files folder holds header files used for communication with SMB- 200 (debug only).
- The debug folder holds the files generated by the Microsoft Visual Studio 6.0 IDE.