버전 선택
MSP-GRLIB
MSP Graphics Library
MSP430GRLIB Package
MSP430GRLIB Image Reformer Utility
제품
MSP430 마이크로컨트롤러
Sub-1GHz 무선 MCU
기타 무선 제품
기타 인터페이스
문서
MSP430 Graphics Library API Guide
새 소식
The following changes have been added to MSP Graphics Library:
- This version of grlib has been updated to be compliant with the CMSIS-Core standard header files for MSP432. Refer to https://www.ti.com/MSP432CMSIS for detailed changes, conversion guide and background information
- The base address/module instance name in MSP432 code examples have been changed from {PERIPHERAL_NAME}_MODULE to {PERIPHERAL_NAME}_BASE per the new device header file definitions. For example TIMER_A0_MODULE to TIMER_A0_BASE
- The driverlib code examples have been updated with the following new files per each IDE requirement
- system_msp432p401r.c
- startup_msp432p401r_ccs.c
- startup_msp432p401r_ewarm.c
출시 정보
The MSP Graphics Library is a royalty-free set of graphics primitives for creating graphical user interfaces on MSP microcontroller-based boards that have a graphical display. The graphical library consists of two building layers of functionality: the display driver layer, specific to the display in use; and the graphics primitives layer, which draws points, lines, rectangles, circles, text, and bitmap images