SBAS661C February 2015 – May 2021 ADS1262 , ADS1263
PRODUCTION DATA
Power-supply rejection ratio (PSRR) is defined as the rejection of the ADC output to the DC change of the power supply voltage referred to the input range. PSRR is calculated using two ADC mean-value readings with inputs shorted, scaled to volts. The first ADC reading (VOA) is acquired at one power-supply voltage, and the second ADC reading (VOB) is acquired after changing the power-supply voltage by 0.5 V. The PSRR calculation is described by Equation 4:
where
For gains > 1, add an additional 6 dB of compensation value for each binary increase of gain.