SBASAS7 August 2024 AMC0106M05
ADVANCE INFORMATION
Place a minimum 10nF capacitor at the device input (from INP to INN). This capacitor helps avoid voltage droop at the input during the sampling period of the switched-capaitor input stage.
Do not leave the inputs of the AMC0106M05 unconnected (floating) when the device is powered up. If either modulator input is left floating, the output bitstream is not valid.
Connect the high-side ground (AGND) to INN, either by a hard short or through a resistive path. A DC current path between INN and AGND is required to define the input common-mode voltage. Do not exceed the input common-mode range, as specified in the Recommended Operating Conditions table. For best accuracy, route the ground connection as a separate trace that connects directly to the sense resistor. Do not short AGND to INN directly at the device input. See the Layout section for more details.