SLUSFJ0 June 2024 BQ51013C-Q1
ADVANCE INFORMATION
Refer to the PDF data sheet for device specific package drawings
PIN | I/O | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
AC1 | 2 | I | AC input from receiver coil. |
AC2 | 19 | I | |
AD | 9 | I | If AD functionality is used, connect this pin to the wired adapter input. When VAD-Pres is applied to this pin wireless charging is disabled and AD_EN is driven low. Connect a 1-µF capacitor from AD to PGND. If unused, the capacitor is not required and AD should be connected directly to PGND. |
AD-EN | 8 | O | Push-pull driver for external PFET when wired charging is active. Float if not used. |
BOOT1 | 3 | O | Bootstrap capacitors for driving the high-side FETs of the synchronous rectifier. Connect a 10-nF ceramic capacitor from BOOT1 to AC1 and from BOOT2 to AC2. |
BOOT2 | 17 | O | |
CHG | 7 | O | Open-drain output – active when OUT is enabled. Float or tie to PGND if unused. |
CLAMP2 | 16 | O | Open-drain FETs which are used for a non-power dissipative overvoltage AC clamp protection. When the RECT voltage goes above 15 V, both switches will be turned on and the capacitors will act as a low impedance to protect the device from damage. If used, capacitors are used to connect CLAMP1 to AC1 and CLAMP2 to AC2. Recommended connections are 0.47-µF capacitors. |
CLAMP1 | 5 | O | |
COMM1 | 6 | O | Open-drain outputs used to communicate with primary by varying reflected impedance. Connect a capacitor from COMM1 to AC1 and a capacitor from COMM2 to AC2 for capacitive load modulation. For resistive modulation connect COMM1 and COMM2 to RECT through a single resistor. See Section 8.3.10 for more information. |
COMM2 | 15 | O | |
EN1 | 10 | I | Inputs that allow user to enable and disable
wireless and wired charging <EN1 EN2>: <00> Wireless charging is enabled unless AD voltage > VAD_Pres. <01> Dynamic communication current limit disabled. <10> AD-EN pulled low, wireless charging disabled. <11> Wired and wireless charging disabled. |
EN2 | 11 | I | |
FOD | 14 | I | Input for the rectified power measurement. See Section 8.3.16 for details. |
ILIM | 12 | I/O | Programming pin for the over current limit. The total resistance from ILIM to GND (RILIM) sets the current limit. The schematic shown in Figure 9-1 illustrates the RILIM as R1 + RFOD. Details can be found in Section 7.5 and Figure 9-1. |
OUT | 4 | O | Output pin, delivers power to the load. |
PGND | 1, 20 | Power ground | |
RECT | 18 | O | Filter capacitor for the internal synchronous rectifier. Connect a ceramic capacitor to PGND. Depending on the power levels, the value may be 4.7 μF to 22 μF. |
TS/CTRL | 13 | I | Dual function
pin: Temperature Sense (TS) and Control (CTRL) pin
functionality. For the TS functionality connect TS/CTRL to ground through a Negative Temperature Coefficient (NTC) resistor. If an NTC function is not desired, connect to PGND with a 10-kΩ resistor. See Section 8.3.13 for more details. For the CTRL functionality pull below VCTRL-Low or pull above VCTRL-High to send an End Power Transfer Packet. See Table 8-4 for more details. |
— | PAD | — | The exposed thermal pad should be connected to ground (PGND) |