SNAS778D June 2021 – July 2024 HDC3020 , HDC3021 , HDC3022
PRODUCTION DATA
Communication to the HDC302x is based upon a command list, which is documented in Table 7-4. Commands other than those documented are undefined and must not be sent to the device.
An I2C write sequence is performed to send a command to the HDC302x. Some of these commands also require configuration data from the I2C controller. In those instances, a CRC byte must accompany the configuration data to permit error checking by the HDC302x. Both of these I2C write scenarios are illustrated in Figure 7-1 and Figure 7-2.