SNAS778C June 2021 – December 2022 HDC3020 , HDC3021 , HDC3022
PRODUCTION DATA
The latest measurement acquisition in Auto Measurement Mode can be retrieved using a measurement readout command, which is documented in Table 8-3, and illustrated in Figure 8-18. Once the measurement readout is complete, the HDC302x clears the measurement result from memory.
As in Section 8.5.7.2, if the I2C controller attempts to read the measurement results prior to measurement completion, the HDC302x will respond with a NACK condition.