SNOSDG3 December 2024 LM74681
PRODUCTION DATA
The enable pin allows for the gate driver to be either enabled or disabled by an external signal. If the EN pin voltage is greater than the rising threshold, the gate drivers and charge pump operates as described in Section 7.3.3 and Section 7.3.2. If the enable pin voltage is less than the input low threshold, the charge pump and gate drivers are disabled placing the LM74681 in shutdown mode. The EN pin to be connected directly to the OUTP pin if enable control is not needed.