SBOSAK0A June 2024 – August 2024 TLV9044-Q1
PRODMIX
The CMRR for the TLV904x-Q1 is specified in several ways so the best match for a given application can be used; see the Electrical Characteristics table. First, the CMRR of the device in the common-mode range below the transition region [VCM < (V+) – 0.7V] is given. This specification is the best indicator of the capability of the device when the application requires using one of the differential input pairs. Second, the CMRR over the entire common-mode range is specified at (VCM = 0V to 5.5V). This last value includes the variations measured through the transition region.