SBOSA15A september 2022 – may 2023 TMP1827
PRODUCTION DATA
The function is issued by the host to copy the scratchpad-1 registers to the EEPROM configuration memory. As shown in Figure 9-22, the temperature alert registers, configuration register, short address register, temperature offset and IO pin configuration registers are stored in the configuration EEPROM. There are 9 bytes being copied from the register space to the NVM, therefore the host must hold the bus in idle state for twice the EEPROM programming time before it performs the next access.