JAJSEC1C November 2019 – July 2020 ADS8686S
PRODUCTION DATA
CHSEL[2:0] are digital input pins.
In hardware mode (HW_RNGSEL[1:0] ≠ 00, SEQEN = 0), these input pins select the channel for the next conversion. See the Section 7.4.2.2.1 section for further details.
In hardware sequence mode (HW_RNGSEL[1:0] ≠ 00, SEQEN = 1), these input pins select the last channel pair in the hardware sequence. See the Section 7.4.2.5.1 section for further details.
In software mode (HW_RNGSEL[1:0] = 00), tie these pin to DGND.