JAJSK08B January 2020 – November 2021 BQ76952
PRODUCTION DATA
The I2C serial communications interface in the BQ76952 device acts as a responder device and supports rates up to 400 kHz with an optional CRC check. If the OTP is not programmed, the BQ76952 device will initially power up by default in 400 kHz I2C mode, although other versions of the device may initially power up in a different mode (as described in the Device Comparison Table. The OTP setting can be programmed on the manufacturing line, then when the device powers up, it automatically enters the selected mode per OTP setting. The host can also change the I2C speed setting while in CONFIG_UPDATE mode, then the new speed setting takes effect upon exit of CONFIG_UPDATE mode. Alternatively, the host can use the SWAP_TO_I2C() subcommand to change the communications interface to I2C immediately.
The I2C device address (as an 8-bit value including responder address and R/W bit) is set by default as 0x10 (write), 0x11 (read), which can be changed by configuration setting.
The communications interface includes programmable timeout capability. This should only be used if the bus will be operating at 100 kHz or 400 kHz. If this is enabled with the device set to 100-kHz mode, then the device will reset the communications interface logic if a clock is detected low longer than a tTIMEOUT of 25 ms to 35 ms, or if the cumulative clock low responder extend time exceeds ≈25 ms, or if the cumulative clock low controller extend time exceeds 10 ms. If the timeouts are enabled with the device set to 400-kHz mode, then the device will reset the communications interface logic if a clock is detected low longer than tTIMEOUT of 5 ms to 20 ms. The bus also includes a long-term timeout if the SCL pin is detected low for more than 2 seconds, which applies whether or not the timeouts above are enabled.
Figure 14-1 shows an I2C write transaction. Block writes are allowed by sending additional data bytes before the Stop. The I2C logic will auto-increment the register address after each data byte.
When enabled, the CRC is calculated as follows:
The CRC polynomial is x8 + x2 + x + 1, and the initial value is 0.
When the responder detects an invalid CRC, the I2C responder NACKs the CRC, which causes the I2C responder to go to an idle state.
Figure 14-2 shows a read transaction using a Repeated Start.
Figure 14-3 shows a read transaction where a Repeated Start is not used; for example, if not available in hardware. For a block read, the controller ACKs each data byte except the last and continues to clock the interface. The I2C block auto-increments the register address after each data byte.
When enabled, the CRC for a read transaction is calculated as follows:
The CRC polynomial is x8 + x2 + x + 1, and the initial value is 0.
When the controller detects an invalid CRC, the I2C controller will NACK the CRC, which causes the I2C responder to go to an idle state.