JAJSMN8D December 2000 – August 2021 DCR021205 , DCR022405
PRODUCTION DATA
The DCR02 can be used to provide a single voltage output by connecting the circuit as shown in Figure 8-1. The ERROR output signal is pulled up to the value of VOUT for the particular DCR02 being used. The value of RERR depends on the loading on the ERROR line; however, the total load on the ERROR line must not exceed the value given in the Section 6.5.
The output can be permanently enabled by connecting the ENABLE pin to the VREC pin. The DCR02 can be enabled remotely by connecting the ENABLE pin to VREC through a pull-up resistor (REN); the value of this resistor is not critical for the DCR02, because only a small current flows. Switch SW1 can be used to pull the ENABLE pin low, thus disabling the output. The switching devices can be a bipolar transistor, FET, or a mechanical device; the main load that it senses is REN.