JAJSBE6D May 2010 – December 2016 DS92LV0421 , DS92LV0422
PRODUCTION DATA.
デバイスごとのパッケージ図は、PDF版データシートをご参照ください。
The DS92LV042x chipset transmits and receives 24 bits of data and 3 control signals, formatted as Channel Link LVDS data, over a single serial CML pair operating at 280 Mbps to 2.1 Gbps. The serial stream contains an embedded clock, video control signals, and the DC-balance information which enhances signal quality and supports AC coupling.
The deserializer can attain lock to a data stream without the use of a separate reference clock source, which greatly simplifies system complexity and overall cost. The deserializer also synchronizes to the serializer regardless of the data pattern, delivering true automatic plug and lock performance. It can lock to the incoming serial stream without the requirement of special training patterns or sync characters. The deserializer recovers the clock and data by extracting the embedded clock information, validating, and then deserializing the incoming data stream, providing a parallel Channel Link LVDS bus to the display, ASIC, or FPGA.
The DS92LV042x chipset can operate with up to 24 bits of raw data with three slower speed control bits encoded within the serial data stream. For applications that require less than the maximum 24 raw data bits per clock cycle, the user must ensure that all unused bit spaces or parallel LVDS channels are set to valid logic states, as all parallel lanes and 27 bit spaces are always sampled.
The DS92LV042x can be configured to accept or transmit 24-bit data with two different LVDS parallel interface mapping schemes:
The mapping schemes can also be selected by register control. The alternate mapping scheme is useful in some applications where the receiving system, typically a display, requires the LSBs for the 24-bit color data to be sent on LVDS Channel 3.
NOTE
While the LVDS parallel interface has 28 bits defined, only 27 bits are recovered by the serializer and sent to the deserializer. This chipset supports 24-bit RGB plus the three video control signals. The 28th bit is not sampled, sent, or recovered.
The DS92LV042x chipset transmits and receives a pixel of data in the following format: C1 and C0 represent the embedded clock in the serial stream. C1 is always high and C0 is always low. The b[23:0] contains the scrambled RGB data. DCB is the DC-Balanced control bit. DCB is used to minimize the short and long-term DC bias on the signal lines. This bit determines if the data is unmodified or inverted. DCA is used to validate data integrity in the embedded data stream and can also contain encoded control (VS, HS, DE). Both DCA and DCB coding schemes are generated by the serializer and decoded by the deserializer automatically. Figure 25 illustrates the serial stream per clock cycle.
NOTE
Figure 25 only illustrates the bits but does not actually represent the bit location, as the bits are scrambled and balanced continuously.
The three control bits can be used to communicate any low speed signal. The most common use for these bits is in the display or machine vision applications. In a display application, these bits are typically assigned as: Bit 26 to DE, Bit 24 to HS, and Bit 25 to VS. In the machine vision standard, Camera Link, these bits are typically assigned: Bit 26 to DVAL, Bit 24 to LVAL, and Bit 25 to FVAL.
When operating the devices in Normal Mode, the video control signals (DE, HS, VS) have the following restrictions:
Glitches of a control signal can cause a visual display error, and video control signals are defined as low frequency signals with limited transitions. Therefore, the video control signal filter feature allows for the chipset to validate and filter out any high frequency noise on the control signals (see Figure 26).
The serializer converts a Channel Link LVDS clock and data bus to a single serial output data stream and also acts as a signal generator for the chipset Built-In Self Test (BIST) mode. The device can be configured through external pins or through the optional serial control bus. The serializer features enhanced signal quality on the link by supporting: a selectable VOD level, a selectable de-emphasis for signal conditioning, and Channel Link II data coding that provides randomization, scrambling, and DC-balancing of the data. The serializer includes multiple features to reduce EMI associated with display data transmission. This includes the randomization and scrambling of the serial data and system spread spectrum clock support. The serializer includes power-saving features with a sleep mode, auto stop clock feature, and optional LVCMOS (1.8 V or 3.3 V) I/O compatibility (see also Optional Serial Bus Control and Built-In Self Test (BIST)).
The serializer differential output voltage may be increased by setting the VODSEL pin high. When VODSEL is low, the DC VOD is at the standard (default) level. When VODSEL is high, the VOD is increased in level. The increased VOD is useful in extremely high noise environments and extra long cable length applications. When using de-emphasis, TI recommends setting VODSEL = H to avoid excessive signal attenuation, especially with the larger de-emphasis settings. This feature may be controlled by external pin or by register.
INPUT | EFFECT | |
---|---|---|
VODSEL | VOD (mV) | VOD (mVp-p) |
L | ±300 | 600 |
H | ±450 | 900 |
The de-emphasis pin controls the amount of de-emphasis beginning one full bit time after a logic transition that the serializer drives. This is useful to counteract loading effects of long or lossy cables. This pin must be left open if used for standard switching currents (no de-emphasis) or if used under register control. De-emphasis is selected by connecting a resistor on this pin to ground, with the R value between 0.5 kΩ and 1 MΩ, or by register setting. When using de-emphasis, TI recommends setting VODSEL = H.
RESISTOR VALUE (kΩ) | DE-EMPHASIS SETTING |
---|---|
Open | Disabled |
0.6 | –12 dB |
1 | –9 dB |
2 | –6 dB |
5 | –3 dB |
Channel Link II serializers and deserializers feature a three-step encoding process that enables the use of AC-coupled interconnects and also helps to manage EMI. The serializer first passes the parallel data through a scrambler which randomizes the data. The randomized data is then DC-balanced. The DC-balanced and randomized data then goes through a bit-shuffling circuit and is transmitted out on the serial line. This encoding process helps to prevent static data patterns on the serial stream. The resulting frequency content of the serial stream ranges from the parallel clock frequency to the Nyquist rate. For example, if the serializer and deserializer chipset is operating at a parallel clock frequency of 50 MHz, the resulting frequency content of the serial stream ranges from 50 MHz to 700 MHz (50 MHz × 28 bits = 1.4 GHz / 2 = 700 MHz).
The serializer RXCLKIN is capable of tracking spread spectrum clocking (SSC) from a host source. The RXCLKIN accepts spread spectrum tracking up to 35-kHz modulation and ±0.5, ±1, or ±2% deviations (center spread). The maximum conditions for the RXCLKIN input are: a modulation frequency of 35 kHz and amplitude deviations of ±2% (4% total).
The serializer has a PDB input pin to enable or power down the device. This pin is controlled by the host and is used to save power, disabling the link when the display is not required. In power-down mode, the high-speed driver outputs are both pulled to VDD and present a 0-V VOD state.
NOTE
In power-down, the optional serial bus control registers are RESET.
The serializer enters a low power SLEEP state when the RXCLKIN is stopped. A STOP condition is detected when the input clock frequency is less than 3 MHz. The clock must be held at a static low or high state. When the RXCLKIN starts again, the serializer locks to the valid input clock and then transmits the serial data to the deserializer.
NOTE
In STOP CLOCK SLEEP, the optional serial bus control registers values are RETAINED.
The serializer parallel control bus can operate with 1.8-V or 3.3-V levels (VDDIO) for host compatibility. The 1.8-V levels offers lower noise (EMI) and also system power savings.
The deserializer converts a single input serial data stream to a Channel Link LVDS clock and data bus and also provides a signal check for the chipset Built-In Self Test (BIST) mode. The device can be configured through external and strap pins or through the optional serial control bus. The deserializer features enhanced signal quality on the link by supporting an integrated equalizer on the serial input and Channel Link II data encoding which provides randomization, scrambling, and DC-balancing of the data. The deserializer includes multiple features to reduce EMI associated with display data transmission. This includes the randomization and scrambling of the data, Channel Link LVDS output interface, and output spread spectrum clock generation (SSCG) support. The deserializer includes power saving features with a power-down mode and optional LVCMOS (1.8-V) interface compatibility.
The deserializer can enable receiver input equalization of the serial stream to increase the eye opening to the deserializer input.
NOTE
This function cannot be seen at the RXIN± input. The equalization feature may be controlled by the external pin or by register.
EQ (STRAP OPTION) | EFFECT |
---|---|
L | ~1.625 dB (OFF) |
H | ~13 dB |
The differential output voltage of the Channel Link parallel interface is controlled by the VODSEL input.
INPUT | EFFECT | |
---|---|---|
VODSEL | VOD (mV) | VOD (mVp-p) |
L | ±250 | 500 |
H | ±400 | 800 |
The deserializer provides access to the center tap of the internal termination. A capacitor may be placed on this pin for additional common-mode filtering of the differential pair. This can be useful in high-noise environments for additional noise rejection capability. A 4.7-µF capacitor may be connected from this pin to Ground.
The deserializer provides an internally generated spread spectrum clock (SSCG) to modulate its outputs. Both clock and data outputs are modulated. This aids to lower system EMI. Output SSCG deviations of ±2% (4% total) at up to 100-kHz modulations are available (see Table 5). This feature may be controlled by external pins or by register.
NOTE
The deserializer supports the SSCG function with TXCLKOUT = 10 MHz to 65 MHz. When the TXCLKOUT = 65 MHz to 75 MHz, it is required to disable the SSCG function (SSC[2:0] = 000).
SSC[2:0] INPUTS
LFMODE = L (20 TO 65 MHz) |
RESULT | |||
---|---|---|---|---|
SSC2 | SSC1 | SSC0 | fdev (%) | fmod (kHz) |
L | L | L | Off | Off |
L | L | H | ±0.9 | CLK/2168 |
L | H | L | ±1.2 | |
L | H | H | ±1.9 | |
H | L | L | ±2.3 | |
H | L | H | ±0.7 | CLK/1300 |
H | H | L | ±1.3 | |
H | H | H | ±1.7 |
SSC[2:0] INPUTS
LFMODE = H (10 TO 20 MHz) |
RESULT | |||
---|---|---|---|---|
SSC2 | SSC1 | SSC0 | fdev (%) | fmod (kHz) |
L | L | L | Off | Off |
L | L | H | ±0.7 | CLK/625 |
L | H | L | ±1.3 | |
L | H | H | ±1.8 | |
H | L | L | ±2.2 | |
H | L | H | ±0.7 | CLK/385 |
H | H | L | ±1.2 | |
H | H | H | ±1.7 |
The deserializer has a PDB input pin to enable or power down the device. This pin can be controlled by the system to save power, disabling the deserializer when the display is not required. An auto-detect mode is also available. In this mode, the PDB pin is tied high and the deserializer enters power-down when the serial stream stops. When the serial stream starts up again, the deserializer locks to the input stream, asserts the LOCK pin, and outputs valid data. In power-down mode, the LVDS data and clock output states are determined by the OSS_SEL status.
NOTE
In power-down, the optional serial bus control registers are RESET.
The deserializer enters a low power SLEEP state when the input serial stream is stopped. A STOP condition is detected when the embedded clock bits are not present. When the serial stream starts again, the deserializer then locks to the incoming signal and recovers the data.
NOTE
In STOP STREAM SLEEP, the optional serial bus control registers values are RETAINED.
The deserializer parallel control bus can operate with 1.8-V or 3.3-V levels (VDDIO) for target (display) compatibility. The 1.8-V levels offers lower noise (EMI) and also system power savings.
When PDB is driven high, the CDR PLL begins locking to the serial input, and LOCK goes from TRI-STATE to low (depending on the value of the OSS_SEL setting). After the DS92LV0422 completes its lock sequence to the input serial data, the LOCK output is driven high, indicating valid data and clock recovered from the serial input is available on the Channel Link outputs. The TXCLKOUT output is held at its current state at the change from OSC_CLK (if this is enabled through OSC_SEL) to the recovered clock (or vice versa).
NOTE
The Channel Link outputs may be held in an inactive state (TRI-STATE) through the use of the Output Enable pin (OEN).
If there is a loss of clock from the input serial stream, LOCK is driven low and the state of the outputs are based on the OSS_SEL setting (configuration pin or register).
INPUTS | OUTPUTS | |||||||
---|---|---|---|---|---|---|---|---|
SERIAL INPUT | PDB | OEN | OSS_SEL | LOCK | OTHER OUTPUTS | |||
X | L | X | X | X | TXCLKOUT is TRI-STATE TXOUT[3:0] are TRI-STATE PASS is TRI-STATE |
|||
Static | H | X | L | L | TXCLKOUT is TRI-STATE TXOUT[3:0] are TRI-STATE PASS is HIGH |
|||
Static | H | L | H | L | TXCLKOUT is TRI-STATE TXOUT[3:0] are TRI-STATE PASS is TRI-STATE |
|||
Static | H | H | H | L | TXCLKOUT is TRI-STATE or Oscillator Output through Register bit TXOUT[3:0] are TRI-STATE PASS is TRI-STATE |
|||
Active | H | L | X | H | TXCLKOUT is TRI-STATE TXOUT[3:0] are TRI-STATE PASS is Active |
|||
Active | H | H | X | H | TXCLKOUT is Active TXOUT[3:0] are Active PASS is Active (Normal operating mode) |
The deserializer provides an optional clock output when the input clock (serial stream) has been lost. This is based on an internal oscillator. The frequency of the oscillator may be selected. This feature may be controlled by external pin or by register.
An optional at-speed Built-In Self Test (BIST) feature supports the testing of the high-speed serial link. This is useful in the prototype stage, equipment production, in-system test, and for system diagnostics. In BIST mode, only an input clock is required along with control to the serializer and deserializer BISTEN input pins. The serializer outputs a test pattern (PRBS-7) and drives the link at speed. The deserializer detects the PRBS-7 pattern and monitors it for errors. A PASS output pin toggles to flag any payloads that are received with 1 to 24 errors. Upon completion of the test, the result of the test is held on the PASS output until reset (new BIST test or power-down). A high on PASS indicates NO ERRORS were detected. A low on PASS indicates one or more errors were detected. The duration of the test is controlled by the pulse width applied to the deserializer BISTEN pin.
Inter-operability is supported between this Channel Link II device and all Channel Link II generations (Gen 1/2/3); see respective data sheets for details on entering BIST mode and control.
See Figure 30 for the BIST mode flow diagram.
Step 1: Place the serializer in BIST Mode by setting serializer BISTEN = H. BIST Mode is enabled through the BISTEN pin. An RXCLKIN is required for BIST. When the deserializer detects the BIST mode pattern and command (DCA and DCB code), the data and control signal outputs are shut off.
Step 2: Place the deserializer in BIST mode by setting the BISTEN = H. The deserializer is now in BIST mode and checks the incoming serial payloads for errors. If an error in the payload (1 to 24) is detected, the PASS pin switches low for one half of the clock period. During the BIST test, the PASS output can be monitored and counted to determine the payload error rate.
Step 3: To stop BIST mode, the deserializer BISTEN pin is set low. The deserializer stops checking the data, and the final test result is held on the PASS pin. If the test ran error free, the PASS output is high. If there is one or more errors detected, the PASS output is low. The PASS output state is held until a new BIST is run, the device is RESET, or powered down. The BIST duration is user controlled by the duration of the BISTEN signal.
Step 4: To return the link to normal operation, the serializer BISTEN input is set low. The link returns to normal operation.
Figure 31 shows the waveform diagram of a typical BIST test for two cases. Case 1 is error-free, and Case 2 shows one with multiple errors. In most cases, it is difficult to generate errors due to the robustness of the link (differential data transmission and so forth), thus they may be introduced by greatly extending the cable length, faulting the interconnect, or reducing signal condition enhancements (de-emphasis, VODSEL, or Rx equalization).
It is possible to calculate the approximate Bit Error Rate (BER). The following is required:
The BER is less than or equal to one over the product of 24 times the RXCLKIN rate times the test duration. If we assume a 65-MHz clock, a 10-minute (600 seconds) test, and a PASS, the BER is ≤ 1.07 × 10E-12.
BIST mode runs a check on the data payload bits. The LOCK pin also provides a link status. If the recovery of the C0 and C1 bits does not reconstruct the expected clock signal, the LOCK pin switches low. The combination of the LOCK and at-speed BIST PASS pin provides a powerful tool for system evaluation and performance monitoring.
The serializer and deserializer may also be configured by the use of a serial control bus that is I2C protocol-compatible. By default, the I2C Reg 0x00 = 0x00, and all configuration is set by control or strap pins. Writing Reg 0x00 = 0x01 enables or allows configuration by registers; this overrides the control or strap pins. Multiple devices may share the serial control bus, because multiple addresses are supported (see Figure 32).
The serial bus is comprised of three pins. The SCL is a serial bus clock input. The SDA is the serial bus data input or output signal. Both SCL and SDA signals require an external pullup resistor to VDDIO. For most applications, a 4.7-kΩ pullup resistor to VDDIO may be used. The resistor value may be adjusted for capacitive loading and data rate requirements. The signals are either pulled high or driven low.
The third pin is the ID[X] pin. This pin sets one of four possible device addresses. Two different connections are possible:
See Table 8 for the serializer and Table 9 for the deserializer. Do not tie ID[X] directly to VSS.
RESISTOR RID kΩ(1) (5% TOL) |
ADDRESS 7'b |
ADDRESS 8'b 0 APPENDED (WRITE) |
---|---|---|
0.47 | 7b' 110 1001 (h'69) | 8b' 1101 0010 (h'D2) |
2.7 | 7b' 110 1010 (h'6A) | 8b' 1101 0100 (h'D4) |
8.2 | 7b' 110 1011 (h'6B) | 8b' 1101 0110 (h'D6) |
Open | 7b' 110 1110 (h'6E) | 8b' 1101 1100 (h'DC) |
RESISTOR RID kΩ(1) (5% TOL) |
ADDRESS 7'b |
ADDRESS 8'b 0 APPENDED (WRITE) |
---|---|---|
0.47 | 7b' 111 0001 (h'71) | 8b' 1110 0010 (h'E2) |
2.7 | 7b' 111 0010 (h'72) | 8b' 1110 0100 (h'E4) |
8.2 | 7b' 111 0011 (h'73) | 8b' 1110 0110 (h'E6) |
Open | 7b' 111 0110 (h'76) | 8b' 1110 1100 (h'EC) |
The serial bus protocol is controlled by START, START-repeated, and STOP phases. A START occurs when SCL transitions low while SDA is high. A STOP occurs when SDA transitions high while SCL is also high (see Figure 33).
To communicate with a remote device, the host controller (master) sends the slave address and listens for a response from the slave. This response is referred to as an acknowledge bit (ACK). If a slave on the bus is addressed correctly, it Acknowledges (ACKs) the master by driving the SDA bus low. If the address doesn't match the slave address of a device, it Not-acknowledges (NACKs) the master by letting SDA be pulled high. ACKs also occur on the bus when data is being transmitted. When the master is writing data, the slave ACKs after every data byte is successfully received. When the master is reading data, the master ACKs after every data byte is received to let the slave know it wants to receive another data byte. When the master wants to stop reading, it NACKs after the last data byte and creates a stop condition on the bus. All communication on the bus begins with either a start condition or a repeated start condition. All communication on the bus ends with a stop condition. A READ is shown in Figure 34 and a WRITE is shown in Figure 35.
NOTE
During initial power-up, a delay of 10 ms is required before the I2C responds.
If the serial bus is not required, the three pins may be left open (NC).
The DS92LV042x chipset is compatible with other single serial lane Channel Link II or FPD-Link II devices. Configuration modes are provided for reverse compatibility with the DS90C241 or DS90C124 chipset (FPD-Link II Generation 1) and also the DS90UR241 / DS90UR124 chipset (FPD-Link II Generation 2) by setting the respective mode with the CONFIG[1:0] pins on the serializer or deserializer as shown in Table 10 and Table 11. This selection also determines whether the control signal filter feature is enabled or disabled in the normal mode. This feature may be controlled by external pin or by register.
CONFIG1 | CONFIG0 | MODE | COMPATIBLE DESERIALIZER DEVICE |
---|---|---|---|
L | L | Normal Mode, Control Signal Filter disabled | DS92LV0422, DS92LV0412, DS92LV2422, DS92LV2412 |
L | H | Normal Mode, Control Signal Filter enabled | DS92LV0422, DS92LV0412, DS92LV2422, DS92LV2412 |
H | L | Reverse Compatibility Mode (FPD-Link II, GEN2) | DS90UR124, DS99R124Q-Q1 |
H | H | Reverse Compatibility Mode (FPD-Link II, GEN1) | DS90C124 |
CONFIG1 | CONFIG0 | MODE | COMPATIBLE SERIALIZER DEVICE |
---|---|---|---|
L | L | Normal Mode, Control Signal Filter disabled | DS92LV0421, DS92LV0411, DS92LV2421, DS92LV2411 |
L | H | Normal Mode, Control Signal Filter enabled | DS92LV0421, DS92LV0411, DS92LV2421, DS92LV2411 |
H | L | Reverse Compatibility Mode (FPD-Link II, GEN2) | DS90UR241, DS99R421 |
H | H | Reverse Compatibility Mode (FPD-Link II, GEN1) | DS90C241 |
ADD (DEC) |
ADD (HEX) |
REGISTER NAME | BIT(S) | R/W | DEFAULT (BIN) |
FUNCTION | DESCRIPTION |
---|---|---|---|---|---|---|---|
0 | 0 | Serializer Config 1 |
7 | R/W | 0 | Reserved | Reserved |
6 | R/W | 0 | MAPSEL | 0: LSB on RXIN3 1: MSB on RXIN3 |
|||
5 | R/W | 0 | VODSEL | 0: Low 1: High |
|||
4 | R/W | 0 | Reserved | Reserved | |||
3:2 | R/W | 00 | CONFIG | 00: Normal Mode, Control Signal Filter Disabled 01: Normal Mode, Control Signal Filter Enabled 10: DS90UR124, DS99R124Q-Q1 Reverse-Compatibility Mode (FPD-Link II, GEN2) 11: DS90C124 Reverse-Compatibility Mode (FPD-Link II, GEN1) |
|||
1 | R/W | 0 | SLEEP | Note – not the same function as PowerDown (PDB) 0: Normal Mode 1: Sleep Mode – Register settings retained. |
|||
0 | R/W | 0 | REG | 0: Configurations set from control pins 1: Configuration set from registers (except I2C_ID) |
|||
1 | 1 | Device ID | 7 | R/W | 0 | REG ID | 0: Address from ID[X] Pin 1: Address from Register |
6:0 | R/W | 1101000 | ID[X] | Serial Bus Device ID, four IDs are: 7b '1101 001 (h'69) 7b '1101 010 (h'6A) 7b '1101 011 (h'6B) 7b '1101 110 (h'6E) All other addresses are reserved. |
|||
2 | 2 | De-Emphasis Control | 7:5 | R/W | 000 | De-Emphasis Setting | 000: set by external resistor 001: –1 dB 010: –2 dB 011: –3.3 dB 100: –5 dB 101: –6.7 dB 110: –9 dB 111: –12 dB |
4 | R/W | 0 | De-Emphasis EN | 0: De-emphasis Enabled 1: De-emphasis Disabled |
|||
3:0 | R/W | 0000 | Reserved | Reserved |
ADD (DEC) |
ADD (HEX) |
REGISTER NAME | BIT(S) | R/W | DEFAULT (BIN) |
FUNCTION | DESCRIPTION |
---|---|---|---|---|---|---|---|
0 | 0 | Deserializer Config 1 | 7 | R/W | 0 | LFMODE | 0: 20 to 65 MHz SSCG Operation 1: 10 to 20 MHz SSCG Operation |
6 | R/W | 0 | MAPSEL | Channel Link Map Select 0: LSB on TXOUT3± 1: MSB on TXOUT3± |
|||
5 | R/W | 0 | Reserved | Reserved | |||
4 | R/W | 0 | Reserved | Reserved | |||
3:2 | R/W | 00 | CONFIG | 00: Normal Mode, Control Signal Filter Disabled 01: Normal Mode, Control Signal Filter Enabled 10: DS90UR241, DS99R421 Reverse-Compatibility Mode (FPD-Link II, GEN2) 11: DS90C241 Reverse-Compatibility Mode (FPD-Link II, GEN1) |
|||
1 | R/W | 0 | SLEEP | Note – not the same function as PowerDown (PDB) 0: Normal Mode 1: Sleep Mode – Register settings retained. |
|||
0 | R/W | 0 | REG Control | 0: Configurations set from control or strap pins 1: Configuration set from registers (except I2C_ID) |
|||
1 | 1 | Device ID | 7 | R/W | 0 | REG ID | 0: Address from ID[X] Pin 1: Address from Register |
6:0 | R/W | 1110000 | ID[X] | Serial Bus Device ID, four IDs are: 7b' 111 0001 (h'71) 7b' 111 0010 (h'72) 7b' 111 0011 (h'73) 7b' 111 0110 (h'76) All other addresses are reserved. |
|||
2 | 2 | Deserializer Features 1 | 7 | R/W | 0 | OEN | Output Enable Input See Table 7 |
6 | R/W | 0 | OSS_SEL | Output Sleep State Select See Table 7 |
|||
5:4 | R/W | 00 | Reserved | Reserved | |||
3 | R/W | 0 | VODSEL | Differential LVDS Driver Output Voltage Select 0: LVDS VOD is ±250 mV, 500 mVp-p (typ) 1: LVDS VOD is ±400 mV, 800 mVp-p (typ) |
|||
2:0 | R/W | 000 | OSC_SEL | 000: OFF 001: Reserved 010: 25 MHz ± 40% 011: 16.7 MHz ± 40% 100: 12.5 MHz ± 40% 101: 10 MHz ± 40% 110: 8.3 MHz ± 40% 111: 6.3 MHz ± 40% |
|||
3 | 3 | Deserializer Features 2 | 7:5 | R/W | 000 | EQ Gain | 000: ~1.625 dB 001: ~3.25 dB 010: ~4.87 dB 011: ~6.5 dB 100: ~8.125 dB 101: ~9.75 dB 110: ~11.375 dB 111: ~13 dB |
4 | R/W | 0 | EQ Enable | 0: EQ = disabled 1: EQ = enabled |
|||
3 | R/W | 0 | Reserved | Reserved | |||
2:0 | R/W | 000 | SSC | If LFMODE = 0 then: 000: SSCG OFF 001: fdev = ±0.9%, fmod = CLK/2168 010: fdev = ±1.2%, fmod = CLK/2168 011: fdev = ±1.9%, fmod = CLK/2168 100: fdev = ±2.3%, fmod = CLK/2168 101: fdev = ±0.7%, fmod = CLK/1300 110: fdev = ±1.3%, fmod = CLK/1300 111: fdev = ±1.7%, fmod = CLK/1300 If LFMODE = 1, then: 001: fdev = ±0.7%, fmod = CLK/625 010: fdev = ±1.3%, fmod = CLK/625 011: fdev = ±1.8%, fmod = CLK/625 100: fdev = ±2.2%, fmod = CLK/625 101: fdev = ±0.7%, fmod = CLK/385 110: fdev = ±1.2%, fmod = CLK/385 111: fdev = ±1.7%, fmod = CLK/385 |