SLVS047L November 1981 – January 2015 LM237 , LM337
PRODUCTION DATA.
NOTE
Information in the following applications sections is not part of the TI component specification, and TI does not warrant its accuracy or completeness. TI’s customers are responsible for determining suitability of components for their purposes. Customers should validate and test their design implementation to confirm system functionality.
This application uses the LMx37 device's reference voltage, combined with the series resistor RS, to limit the current to 1.25 V ÷ RS
VO is determined by the values of R1 and R2. Choosing R1 = 120 Ω means that about 10.42 mA of current will flow through R1. The ~10 mA of current satisfies the minimum operating current and renders IREF negligible. Since the current is coming from ground, the same amount of current will flow through R2. Therefore, the size of R2 will be the dominant factor in adjusting VO. The relationship between R1, R2, and VO is as follows:
where