JAJSML9K April 2006 – December 2024 LP2950 , LP2951
PRODUCTION DATA
VOUT is set by the external feedback resistors R1 and R2 according to the following equation:
To ignore the FB pin current error term in the VOUT equation, set the feedback divider current to 100 times the FB pin current listed in the Section 5.5 table. This setting provides the maximum feedback divider series resistance, as shown in the following equation: