SLLSEO4A June 2015 – July 2015 ONET1130EP
PRODUCTION DATA.
A simplified block diagram of the ONET1130EP is shown in Functional Block Diagram.
The ONET1130EP consists of a transmitter path, a receiver path, an analog reference block, an analog to digital converter and a 2-wire serial interface and control logic block with power-on reset.
The transmit path consists of an adjustable input equalizer, and an output modulator driver. The output driver provides a differential output voltage but can be operated in a single-ended mode to reduce the power consumption. Output waveform control, in the form of cross-point adjustment and de-emphasis are available to improve the optical eye mask margin. Bias current for the laser is provided and an integrated automatic power control (APC) loop to compensate for variations in average optical power over voltage, temperature and time is included.
The receive path consists of a limiting amplifier with programmable equalization and threshold adjustment, and an output driver with de-emphasis to compensate for frequency dependent loss of connectors and transmission lines. The receiver output amplitude, de-emphasis and loss of signal assert level can be adjusted.
The ONET1130EP contains an analog to digital converter to support transceiver digital diagnostics and can report the supply voltage, laser bias current, laser photodiode current and internal temperature.
The 2-wire serial interface is used to control the operation of the device and read the status of the control registers.
The device contains internal EEPROM for trimming purposes only.
The data signal is applied to an input equalizer by means of the input signal pins TXIN+ / TXIN–, which provide on-chip differential 100-Ω line termination. The equalizer is enabled by default and can be disabled by setting the transmitter equalizer disable bit TXEQ_DIS = 1 (bit 1 of register 10). Equalization of up to 300 mm (12 inches) of microstrip or stripline transmission line on FR4 printed circuit boards can be achieved. The amount of equalization is set through register settings TXCTLE [0..3] (register 11). The device can accept input amplitude levels from 100 mVpp up to 1000 mVpp.
The modulation current is sunk from the common emitter node of the limiting output driver differential pair by means of a modulation current generator, which is digitally controlled by the 2-wire serial interface.
The collector nodes of the output stages are connected to the transmitter output pins TXOUT+ and TXOUT–. The collectors have internal 50Ω back termination resistors to VCC_TX. The outputs are optimized to drive a 50 Ω single-ended load and to obtain the maximum single-ended output voltage of 2.0Vpp, AC coupling and inductive pull-ups to VCC are required. For reduced power consumption the DC resistance of the inductive pull-ups should be minimized to provide sufficient headroom on the TXOUT+ and TXOUT– pins.
The polarity of the output pins can be inverted by setting the transmitter output polarity switch bit, TXOUTPOL (bit 5 of register 10) to 1. In addition, the output driver can be disabled by setting the transmitter output driver disable bit TXOUT_DIS = 1 (bit 6 of register 10).
The output driver is set to differential output by default. In order to reduce the power consumption for single-ended applications driving an electroabsorptive modulated laser (EML) the output drive register 13 should be set to single-ended mode. The single-ended output signal is enabled by setting the transmitter mode select bit TXMODE = 1 (bit 6 of register 13). The positive output is active by default. To enable the negative output and disable the positive output set TXOUTSEL = 1 (bit 7 of register 13).
Output de-emphasis can be applied to the signal by adjusting the transmitter de-emphasis bits TXDEADJ[0..3] (bits 0 to 3 of register 13). In addition, the width of the applied de-emphasis can be increased by setting the transmitter output peaking width TXPKSEL = 1 (bit 6 of register 11). The wide peaking width would typically be useful for a more capacitive transmitter load. How de-emphasis is applied is controlled through the TXSTEP bit (bit 5 of register 13). Setting TXSTEP = 1 delays the time of the applied de-emphasis and has more of an impact on the falling edge. A graphical representation of the two de-emphasis modes is shown in Figure 34. Using de-emphasis can help to optimize the transmitted output signal; however, it will add to the power consumption.
The output edge speed can be set to slow mode of operation through the TXSLOW bit (bit 4 of register 13). For transmitter modulation output settings (TXMOD - register 12) below 0xC0 it is recommended to set TXSLOW = 1 to reduce the output jitter.
The modulation current generator provides the current for the high speed output driver described above. The circuit can be digitally controlled through the 2-wire interface block or controlled by applying an analog voltage in the range of 0 to 2V to the AMP pin. The default method of control is through the 2-wire interface. To use the AMP pin set the transmitter amplitude control bit TXAMPCTRL = 1 (bit 0 of register 10).
An 8-bit wide control bus, TXMOD[0..7] (register 12), is used to set the desired modulation current and the output voltage.
The entire transmitter signal path,, can be disabled and powered down by setting TX_DIS = 1 (bit 7 of register 10).
The ONET1130EP transmitter has DC offset cancellation to compensate for internal offset voltages. The offset cancellation can be disabled by setting TXOC_DIS = 1 (bit 2 of register 10).
The crossing point can be moved toward the one level by setting TXCPSGN = 1 (bit 7 of register 14) and it can be moved toward the zero level by setting TXCPSGN = 0. The percentage of shift depends upon the register settings of the transmitter cross-point adjustment bits TXCPADJ[0..6] (register 14).
The signal input to the TXIN+ and TXIN– pins can be looped back to the receiver output as shown in Figure 35 by setting TX_LBMUX = 1 (bit 0 of register 2). Loopback from the receiver input to the transmitter output (optical loopback) can be enabled at the same time.
The bias current for the laser is turned off by default and has to be enabled by setting the laser bias current enable bit TXBIASEN = 1 (bit 2 of register 1). In open loop operation, selected by setting TXOLENA = 1 (bit 4 of register 1), the bias current is set directly by the 10-bit wide control word TXBIAS[0..9] (register 15 and register 16). In Automatic Power Control (APC) mode, selected by setting TXOLENA = 0, the bias current depends on the register settings TXBIAS[0..9] and the coupling ratio (CR) between the laser bias current and the photodiode current. CR = IBIAS/IPD. If the photodiode cathode is connected to VCC and the anode is connected to the PD pin (PD pin is sinking current) set TXPDPOL = 1 (bit 0 of register 1). If the photodiode anode is connected to ground and the cathode is connected to the PD pin (PD pin is sourcing current), set TXPDPOL = 0.
Three photodiode current ranges can be selected by means of the photodiode current range bits TXPDRNG[0..1] (bits 5 and 6 of register 1). The photodiode range should be chosen to keep the laser bias control DAC, TXBIAS[0..9], close to the center of its range. This keeps the laser bias current set point resolution high. For details regarding the bias current setting in open-loop mode as well as in closed-loop mode, see the Register Mapping table.
The ONET1130EP has the ability to source or sink the bias current. The default condition is for the BIAS pin to source the current (TXBIASPOL = 0). To act as a sink, set TXBIASPOL = 1 (bit 1 of register 1).
The bias current is monitored using a current mirror with a gain equal to 1/100. By connecting a resistor between MONB and GND, the bias current can be monitored as a voltage across the resistor. A low temperature coefficient precision resistor should be used. The bias current can also be monitored as a 10 bit unsigned digital word by setting the transmitter bias current digital monitor selection bit TXDMONB = 1 (bit 5 of register 16) and removing the resistor from MONB to ground.
The photodiode current is monitored using a current mirror with various gains that are dependent upon the photodiode current range being used. By connecting a resistor between MONP and GND, the photodiode current can be monitored as a voltage across the resistor. A low temperature coefficient precision resistor should be used. The photodiode current can also be monitored as a 10 bit unsigned digital word by setting the transmitter photodiode current digital monitor selection bit TXDMONP = 1 (bit 6 of register 16) and removing the resistor from MONP to ground.
The ONET1130EP provides built in laser safety features. The following fault conditions are detected if the transmitter fault detection enable bit TXFLTEN = 1 (bit 3 of register 1):
If the fault detection is being used then to avoid a fault from occurring at start-up it is recommended to set up the required bias current and APC loop conditions first and enable the laser bias current (TXBIASEN = 1) as the last step in the sequence of commands.
If one or more fault conditions occur and the transmitter fault enable bit TXFLTEN is set to 1, the ONET1130EP responds by:
Fault recovery is performed by the following procedure:
The data signal is applied to an input equalizer by means of the input signal pins RXIN+ / RXIN–, which provide on-chip differential 100 Ω line-termination. The equalizer is enabled by default and can be disabled by setting the receiver equalizer disable bit RXEQ_DIS = 1 (bit 1 of register 4). Equalization is provided for bandwidth compensation of the optical receiver. The amount of equalization is set through the register settings RXCTLE [0..2] (register 5). The device can accept input amplitude levels from 6 mVpp up to 800 mVpp.
Receiver offset cancellation compensates for internal offset voltages and thus ensures proper operation even for very small input data signals. The offset cancellation is enabled by default and the input threshold voltage can be adjusted using register settings RXTHADJ[0..3] (register 6) to optimize the bit error rate or change the eye crossing point to compensate for input signal pulse width distortion. The offset cancellation can be disabled by setting RXOC_DIS = 1 (bit 2 of register 4) and this also disables the cross point adjustment.
The output amplitude of the driver can be varied from 300 mVpp to 900 mVpp using the register settings RXAMP[0..3] (register 8). The default amplitude setting is 300 mVpp. To compensate for frequency dependent losses of transmission lines connected to the output, adjustable de-emphasis is provided. The de-emphasis can be adjusted using RXDADJ[0..2] (register 8). The polarity of the output pins can be inverted by setting the receiver output polarity switch bit RXOUTPOL = 1 (bit 5 of register 4).
In addition, the output driver can be disabled by setting the receiver output driver disable bit RXOUT_DIS = 1 (bit 6 of register 4) or the receiver signal path can be disabled and powered down by setting RX_DIS = 1 (bit 7 of register 4).
The signal input to the RXIN+ and RXIN– pins can be looped back to the transmitter output as shown in Figure 36 by setting RX_LBMUX = 1 (bit 1 of register 2). Loopback from the transmitter input to the receiver output (electrical loopback) can be enabled at the same time.
The loss of signal (LOS) detection is done by 2 separate level detectors to cover a wide dynamic range. The peak values of the input signal are monitored by a peak detector and compared to a pre-defined loss of signal threshold voltage inside the loss of signal detection block. As a result of the comparison, the LOS signal, which indicates that the input signal amplitude is below the defined threshold level, is generated. There are 2 LOS ranges settable with the RXLOSRNG bit (bit 0 of register 4). With RXLOSRNG = 0 the high range of the LOS assert values are used (40 mVPP to 130 mVPP) and by setting RXLOSRNG = 1 the low range of the LOS assert values are used (10 mVPP to 50 mVPP). There are 64 possible internal LOS settings set with RXLOSA[0..5] (register 7) for each LOS range to adjust the LOS assert level.
The typical LOS hysteresis, as defined by 20log(LOS de-assert voltage/LOS assert voltage) is 4 dB. This can be reduced by approximately 2 dB by setting receiver hysteresis RXHYS = 1 (bit 7 of register 6). In addition, the LOS detection time can be reduced by setting the receiver fast LOS bit RXFLOS = 1 (bit 3 of register 5); however, this may result in chatter (LOS bounce).
The ONET1130EP is supplied by a single 2.5 V ±5% supply voltage connected to the VCC_TX, VCC_RX and VDD pins. This voltage is referred to ground (GND) and can be monitored as a 10 bit unsigned digital word through the 2-wire interface.
On-chip bandgap voltage circuitry generates a reference voltage, independent of the supply voltage, from which all other internally required voltages and bias currents are derived.
In order to minimize the module component count, the ONET1130EPprovides an on-chip temperature sensor. The temperature can be monitored as a 10 bit unsigned digital word through the 2-wire interface.
The ONET1130EP has power on reset circuitry which ensures that all registers are reset to default values during startup. After the power-on to initialize time (tINIT1), the internal registers are ready to be loaded. The part is ready to transmit data after the initialize to transmit time (tINIT2), assuming that the enable chip bit EN_CHIP = 1 (bit 0 of register 0). In addition, the transmitter disable pin TX_DIS and receiver disable pin RX_DIS must be set to zero.
The ONET1130EP bias current can be disabled by setting the TX_DIS pin high. The internal registers are not reset. After the transmitter disable pin TX_DIS is set low the part returns to its prior output settings.
The ONET1130EP has an internal 10 bit analog to digital converter (ADC) that converts the analog monitors for temperature, power supply voltage, bias current and photodiode current into a 10 bit unsigned digital word. The first 8 most significant bits (MSBs) are available in register 40 and the 2 least significant bits (LSBs) are available in register 41. Depending on the accuracy required, 8 bits or 10 bits can be read. However, due to the architecture of the 2-wire interface, in order to read the 2 registers, 2 separate read commands have to be sent.
The ADC is enabled by default so to monitor a particular parameter, select the parameter with ADCSEL[0..2] (bits 0 to 2 of register 3). Table 2 shows the ADCSEL bits and the parameter that is monitored.
ADCSEL2 | ADCSEL1 | ADCSEL0 | MONITORED PARAMETER |
---|---|---|---|
0 | 0 | 0 | Temperature |
0 | 0 | 1 | Supply voltage |
0 | 1 | 0 | Bias current |
0 | 1 | 1 | Photodiode current |
To digitally monitor the photodiode current, ensure that TXDMONP = 1 (bit 6 of register 16) and that a resistor is not connected to the MONP pin. To digitally monitor the bias current, ensure that TXDMONB = 1 (bit 5 of register 16) and that a resistor is not connected to the MONB pin. The ADC is disabled by default. To enable the ADC, set the ADC oscillator enable bit OSCEN = 1 (bit 6 of register 3) and set the ADC enable bit ADCEN = 1 (bit 7 of register 3).
The digital word read from the ADC can be converted to its analog equivalent through the following formulas.
Where: ADCx = the decimal value read from the ADC
The ONET1130EP uses a 2-wire serial interface for digital control. The two circuit inputs, SDA and SCK, are driven, respectively, by the serial data and serial clock from a microprocessor, for example. The SDA and SCK pins require external 4.7-kΩ to 10-kΩ pull-up resistor to VCC for proper operation.
The 2-wire interface allows write access to the internal memory map to modify control registers and read access to read out the control signals. The ONET1130EP is a slave device only which means that it cannot initiate a transmission itself; it always relies on the availability of the SCK signal for the duration of the transmission. The master device provides the clock signal as well as the START and STOP commands. The protocol for a data transmission is as follows:
Regarding timing, the ONET1130EP is I2C compatible. The typical timing is shown in Figure 1 and a complete data transfer is shown in Figure 37. Parameters for Figure 1 are defined in Table 1.
Both SDA and SCK lines remain HIGH
A change in the state of the SDA line, from HIGH to LOW, while the SCK line is HIGH, defines a START condition (S). Each data transfer is initiated with a START condition.
A change in the state of the SDA line from LOW to HIGH while the SCK line is HIGH defines a STOP condition (P). Each data transfer is terminated with a STOP condition; however, if the master still wishes to communicate on the bus, it can generate a repeated START condition and address another slave without first generating a STOP condition.
Only one data byte can be transferred between a START and a STOP condition. The receiver acknowledges the transfer of data.
Each receiving device, when addressed, is obliged to generate an acknowledge bit. The transmitter releases the SDA line and a device that acknowledges must pull down the SDA line during the acknowledge clock pulse in such a way that the SDA line is stable LOW during the HIGH period of the acknowledge clock pulse. Setup and hold times must be taken into account. When a slave-receiver doesn’t acknowledge the slave address, the data line must be left HIGH by the slave. The master can then generate a STOP condition to abort the transfer. If the slave-receiver does acknowledge the slave address but some time later in the transfer cannot receive any more data bytes, the master must abort the transfer. This is indicated by the slave generating the not acknowledge on the first byte to follow. The slave leaves the data line HIGH and the master generates the STOP condition, see Figure 1.
The ONET1130EP has two main functional modes of operation: differential transmitter output and single-ended transmitter output.
Operation with differential output is the default mode of operation. This mode is intended for externally modulated lasers requiring differential drive such as Mach Zehnder modulators.
In order to reduce the power consumption for single-ended EML applications the output driver should be set to single-ended mode. The single-ended output signal can be enabled by setting the transmitter mode select bit TXMODE = 1 (bit 6 of register 13). The positive output is active by default. To enable the negative output and disable the positive output set TXOUTSEL = 1 (bit 7 of register 13).
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | Reserved | 0 | 1 | ||||
RWSC | RW | – | – | – | RWSC | RWSC | RW |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset. RWSC = Read/Write self clearing (always reads back to zero) |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | GLOBAL SW_PIN RESET | RWSC | 0h | Global Reset SW
1 = reset, resets all I2C and EEPROM modules to default 0 = normal operation (self-clearing, always reads back ‘0’) |
6 :2 | – | R/W | 4h | Reserved |
1 | I2C RESET | RWSC | 0h | Chip reset bit
1 = resets all I2C registers to default 0 = normal operation (self-clearing, always reads back ‘0’) |
0 | EN_CHIP | R/W | 1h | Enable chip bit
1 = Chip enabled |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | TXMONPFLT | R/W | 0 | Analog photodiode current monitor fault trigger bit 1 = Fault trigger on MONP pin is enabled 0 = Fault trigger on MONP pin is disabled |
6 5 |
TXPDRNG1 TXPDRNG0 |
R/W | 0 | Photodiode current range bits
1X: up to 3080μA / 3μA resolution 01: up to 1540μA / 1.5μA resolution 00: up to 770μA / 0.75μA resolution |
4 | TXOLENA | R/W | 0 | Open loop enable bit
1 = Open loop bias current control 0 = Closed loop bias current control |
3 | TXFLTEN | R/W | 0 | Fault detection enable bit
1 = Fault detection on 0 = Fault detection off |
2 | TXBIASEN | R/W | 0 | Laser Bias current enable bit
1 = Bias current enabled. Toggle to 0 to reset a fault condition. 0 = Bias current disabled |
1 | TXBIASPOL | R/W | 0 | Laser Bias current polarity bit
1 = Bias pin sinks current 0 = Bias pin sources current |
0 | TXPDPOL | R/W | 0 | Photodiode polarity bit
1 = Photodiode cathode connected to VCC 0 = Photodiode anode connected to GND |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Reserved | 0 | 0 | |||||
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7:4 | – | R/W | 0h | Reserved |
3 | – | R/W | 0h | Reserved |
2 | – | R/W | 0h | Reserved |
1 | RX_LBMUX | R/W | 0h | RX-Loopback MUX Setting (optical LB)
1 = Loopback from TX output selected. 0 = Normal operation: RX output selected |
0 | TX_LBMUX | R/W | 0h | TX-Loopback MUX Setting (electrical LB)
1 = Loopback from RX output selected. 0 = Normal operation: TX output selected |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | – | 0 | – | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | ADCEN | R/W | 0h | ADC enabled bit
1 = ADC enabled 0 = ADC disabled |
6 | OSCEN | R/W | 0h | ADC oscillator bit
1 = Oscillator enabled 0 = Oscillator disabled |
5 | – | R/W | 0h | Reserved |
4 | ADCRST | R/W | 0h | ADC reset
1 = ADC reset 0 = ADC no reset |
3 | – | R/W | 0h | Reserved |
2 | ADCSEL2 | R/W | 0h | ADC input selection bits <2:0>
000 selects the temperature sensor 001 selects the power supply monitor 010 selects IMONB 011 selects IMONP 1XX are reserved |
1 | ADCSEL1 | R/W | 0h | |
0 | ADCSEL0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | – | – | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | RX_DIS | R/W | 0h | RX disable bit
1 = RX disabled (power-down) 0 = RX enabled |
6 | RXOUT_DIS | R/W | 0h | RX Output Driver disable bit
1 = output driver is disabled 0 = output driver is enabled |
5 | RXOUTPOL | R/W | 0h | RX Output polarity switch bit
1 = inverted polarity 0 = normal polarity |
4:3 | – | R/W | 0h | Reserved |
2 | RXOC_DIS | R/W | 0h | RX Offset cancellation disable bit
1 = offset cancellation and threshold adjust is disabled 0 = offset cancellation and threshold adjust is enabled |
1 | RXEQ_DIS | R/W | 0h | RX Equalizer disable bit
1 = RX Equalizer is disabled and bypassed 0 = RX Equalizer is enabled |
0 | RXLOSRNG | R/W | 0h | LOS range bit
1 = low LOS assert voltage range 0 = high LOS assert voltage range |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Reserved | 0 | 0 | 0 | 0 | |||
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7:4 | – | R/W | 0h | Reserved |
3 | RXFLOS | R/W | 0h | Receiver fast LOS bit
1 = Fast LOS 0 = normal operation |
2 | RXCTLE2 | R/W | 0h | RX input CTLE setting
000 = minimum 111 = maximum |
1 | RXCTLE1 | R/W | 0h | |
0 | RXCTLE0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | Reserved | 0 | 0 | 0 | 0 | 0 | |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | RXHYS | R/W | 0h | Receiver Hysteresis
1 = Reduce hysteresis level by approximately 2dB 0 = default level of hysteresis (approximately 4dB) |
6:5 | – | R/W | 0h | Reserved |
4 | RXTHSGN | R/W | 0h | RX Eye cross-point adjustment setting
RXTHSGN = 1 (positive shift) Maximum shift for 1111 Maximum shift for 1111 |
3 | RXTHADJ3 | R/W | 0h | |
2 | RXTHADJ2 | R/W | 0h | |
1 | RXTHADJ1 | R/W | 0h | |
0 | RXTHADJ0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Reserved | 0 | 0 | 0 | 0 | 0 | 0 | |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7:6 | – | R/W | 0h | Reserved |
5 | RXLOSA5 | R/W | 0h | LOS assert level
Minimum LOS assert level for 000000 Maximum LOS assert level for 111111 |
4 | RXLOSA4 | R/W | 0h | |
3 | RXLOSA3 | R/W | 0h | |
2 | RXLOSA2 | R/W | 0h | |
1 | RXLOSA1 | R/W | 0h | |
0 | RXLOSA0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Reserved | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | – | R/W | 0h | Reserved |
6 | RXDADJ1 | R/W | 0h | RX output de-emphasis setting
00 = minimum de-emphasis 11 = maximum de-emphasis |
5 | RXDADJ0 | R/W | 0h | |
4 | RXDRVSC | R/W | 0h | RX driver short circuit protection
1 = short circuit protection enabled 0 = normal operation |
3 | RXAMP3 | R/W | 0h | RX output amplitude adjustment
0000 = minimum amplitude 1111 = maximum amplitude |
2 | RXAMP2 | R/W | 0h | |
1 | RXAMP1 | R/W | 0h | |
0 | RXAMP0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Reserved | |||||||
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 :1 | – | R/W | 0h | Reserved |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | – | – | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | TX_DIS | R/W | 0h | TX disable bit
1 = TX disabled (power-down) 0 = TX enabled |
6 | TXOUT_DIS | R/W | 0h | TX Output Driver disable bit
1 = output disabled 0 = output enabled |
5 | TXOUTPOL | R/W | 0h | TX Output polarity switch bit
1 = inverted polarity 0 = normal polarity |
4:3 | – | R/W | 0h | Reserved |
2 | TXOC_DIS | R/W | 0h | TX OC disable bit
1 = TX Offset Cancellation disabled 0 = TX Offset Cancellation enabled |
1 | TXEQ_DIS | R/W | 0h | TX Equalizer disable bit
1 = TX Equalizer is disabled and bypassed 0 = TX Equalizer is enabled |
0 | TXAMPCTRL | R/W | 0h | TX AMP Ctrl
1 = TX AMP Control is enabled (analog amplitude control) 0 = TX AMP Control is disabled (digital amplitude control) |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | TXAMPRNG | R/W | 0h | TX output AMP range
1 = Half TX output amplitude range 0 = Full TX output amplitude range |
6 | TXPKSEL | R/W | 0h | TX output peaking width
1 = wide peaking width 0 = narrow peaking width |
5 | TXTCSEL1 | R/W | 0h | TXOUT temperature compensation select bit 1 |
4 | TXTCSEL0 | R/W | 0h | TXOUT temperature compensation select bit 0 |
3 | TXCTLE3 | R/W | 0h | TX input CTLE setting
0000 = minimum 1111 = maximum |
2 | TXCTLE2 | R/W | 0h | |
1 | TXCTLE1 | R/W | 0h | |
0 | TXCTLE0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | TXMOD7 | R/W | 0h | TX Modulation current setting: sets the output voltage
Output Voltage: 2.4 Vpp / 9.5 mVpp steps |
6 | TXMOD6 | R/W | 0h | |
5 | TXMOD5 | R/W | 0h | |
4 | TXMOD4 | R/W | 0h | |
3 | TXMOD3 | R/W | 0h | |
2 | TXMOD2 | R/W | 0h | |
1 | TXMOD1 | R/W | 0h | |
0 | TXMOD0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | TXOUTSEL | R/W | 0h | TX output selection bit
1 = The negative output TXOUT– is active if TXMODE = 1 0 = The positive output TXOUT+ is active if TXMODE = 1 |
6 | TXMODE | R/W | 0h | TX output mode selection bit
1 = Single-ended mode 0 = Differential mode |
5 | TXSTEP | R/W | 0h | TX output de-emphasis mode selection bit
1 = Delayed de-emphasis 0 = Normal de-emphasis |
4 | TXSLOW | R/W | 0h | TX edge speed selection bit
1 = Slow edge speed 0 = Normal operation |
3 | TXDEADJ3 | R/W | 0h | TX de-emphasis setting
0000 = minimum 1111 = maximum |
2 | TXDEADJ2 | R/W | 0h | |
1 | TXDEADJ1 | R/W | 0h | |
0 | TXDEADJ0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | TXCPSGN | R/W | 0h | TX Eye cross-point adjustment setting
TXCPSGN = 1 (positive shift) Maximum shift for 1111111 Maximum shift for 1111111 |
6 | TXCPADJ6 | R/W | 0h | |
5 | TXCPADJ5 | R/W | 0h | |
4 | TXCPADJ4 | R/W | 0h | |
3 | TXCPADJ3 | R/W | 0h | |
2 | TXCPADJ2 | R/W | 0h | |
1 | TXCPADJ1 | R/W | 0h | |
0 | TXCPADJ0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | TXBIAS9 | R/W | 0h | Bias current settings (8MSB; 2LSBs are in register 16)
Closed loop (APC): Coupling ratio CR = IBIAS / IPD, TXBIAS = 0..1023, IBIAS ≤ 150mA: TXPDRNG = 00; IBIAS = 0.75μA x CR x TXBIAS TXPDRNG = 01; IBIAS = 1.5μA x CR x TXBIAS TXPDRNG = 1X; IBIAS = 3μA x CR x TXBIAS
Open Loop:
|
6 | TXBIAS8 | R/W | 0h | |
5 | TXBIAS7 | R/W | 0 h | |
4 | TXBIAS6 | R/W | 0h | |
3 | TXBIAS5 | R/W | 0h | |
2 | TXBIAS4 | R/W | 0h | |
1 | TXBIAS3 | R/W | 0h | |
0 | TXBIAS2 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Reserved | 0 | 0 | Reserved | 0 | 0 | ||
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | – | R/W | 0h | Reserved |
6 | TXDMONP | R/W | 0h | Digital photodiode current monitor selection bit (MONP)
1 = Digital photodiode monitor is active (no external resistor is needed) 0 = Analog photodiode monitor is active (external resistor is required) |
5 | TXDMONB | R/W | 0h | Digital bias current monitor selection bit (MONB)
1 = Digital bias current monitor is active (no external resistor is needed) 0 = Analog bias current monitor is active (external resistor is required) |
4:2 | – | R/W | 0h | Reserved |
1 | TXBIAS1 | R/W | 0h | Bias current setting (2 LSBs) |
0 | TXBIAS0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | TXBMF7 | R/W | 0h | Bias current monitor fault threshold
With TXDMONB = 1 Register sets the value of the bias current that will trigger a fault. The external resistor on the MONB pin must be removed to use this feature. |
6 | TXBMF6 | R/W | 0h | |
5 | TXBMF5 | R/W | 0h | |
4 | TXBMF4 | R/W | 0h | |
3 | TXBMF3 | R/W | 0h | |
2 | TXBMF2 | R/W | 0h | |
1 | TXBMF1 | R/W | 0h | |
0 | TXBMF0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | TXPMF7 | R/W | 0h | Power monitor fault threshold
With TXDMONP = 1 Register sets the value of the photodiode current that will trigger a fault. The external resistor on the MONP pin must be removed to use this feature. |
6 | TXPMF6 | R/W | 0h | |
5 | TXPMF5 | R/W | 0h | |
4 | TXPMF4 | R/W | 0h | |
3 | TXPMF3 | R/W | 0h | |
2 | TXPMF2 | R/W | 0h | |
1 | TXPMF1 | R/W | 0h | |
0 | TXPMF0 | R/W | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Reserved | |||||||
R/W | R/W | R/W | R/W | R/W | R/W | R/W | R/W |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7:0 | – | – | – | Reserved |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
R | R | R | R | R | R | R | R |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | ADC9 (MSB) | R | 0h |
Digital representation of the ADC input source (read only) |
6 | ADC8 | R | 0h | |
5 | ADC7 | R | 0h | |
4 | ADC6 | R | 0h | |
3 | ADC5 | R | 0h | |
2 | ADC4 | R | 0h | |
1 | ADC3 | R | 0h | |
0 | ADC2 | R | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Reserved | 0 | 0 | |||||
R | R | R | R | R | R | R | R |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7:2 | – | R | 0h | Reserved |
1 | ADC1 | R | 0h | Digital representation of the ADC input source (read only) |
0 | ADC0 (LSB) | R | 0h |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Reverved | 0 | 0 | Reserved | ||||
R | R | R | R | R | R | R | R |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset; RCLR = Read clear |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | – | R | 0 | Reserved |
6 | – | RCLR | 0 | Reserved |
5 | RXLOS | R | 0 | RX LOS status bit 1 = RX LOS asserted 0 = RX LOS de-asserted |
4 | RX_LOS (latched high) | RCLR | 0 | Latched high status of RXLOS(bit5). Cleared when read. Latched high status set to 1 when raw status goes high and keep it high even if raw status goes low. |
3:0 | R | 0 | Reserved |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
R | R | R | R | R | R | R | R |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset; RCLR = Read clear |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7 | – | R | 0 | Reserved |
6 | – | RCLR | 0 | Reserved |
5 | TX_FLT | R | 0 | TX fault status bit
1 = TX fault detected 0 = TX fault not detected |
4 | TX_DRVDIS | R | 0 | TX driver disable status bit
1 = TX fault logic disables the driver 0 = TX fault logic does not disable the driver |
3:0 | – | R | 0 | Reserved |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Reserved | |||||||
R | R | R | R | R | R | R | R |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7:0 | – | – | – | Reserved |
7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
Reserved | |||||||
R | R | R | R | R | R | R | R |
LEGEND: R/W = Read/Write; R = Read only; -n = value after reset |
Bit | Field | Type | Reset | Description |
---|---|---|---|---|
7:0 | – | Reserved |