JAJSH90D April 2019 – June 2022 TMP235-Q1 , TMP236-Q1
PRODUCTION DATA
Depending on the input characteristics of the ADC, an external CFILTER may be required. The value of CFILTER depends on the size of the sampling capacitor (CSAMPLE) and the sampling frequency while observing a maximum CLOAD of 1000 pF. The capacitor requirements can vary because the input stages of all ADCs are not identical. Figure 8-1 shows a general ADC application as an example only.