JAJSL81C february 2021 – july 2023 TMUX7308F , TMUX7309F
PRODUCTION DATA
The image shows the case where an incorrect wiring condition occurred and one of the input connectors has been shorted to the power board supply voltage. If the board supply voltage is higher than the power supply of the multiplexer, then the TMUX7308F or TMUX7309F will disconnect the source input from passing the signal to protect the downstream ADC. The drain pin of the mux will be pulled up to the supply voltage VDD through a 40 kΩ resistor to allow the ADC to determine a fault condition has occurred.