2 改訂履歴
Changes from April 18, 2014 to March 27, 2017
-
Section 1.3、「概要」の内容を変更Go
-
Added Section 3.1, Related Products Go
-
Moved TSTG from Section 5.2 to Section 5.1, Absolute Maximum RatingsGo
-
Added VOL and VOH to Section 5.4, Electrical Characteristics Go
-
Changed the TYP value of the fD_CLKmax parameter from 8 to 4 MHz in Section 5.4, Electrical Characteristics Go
-
Throughout document, removed support for application control of Automatic Gain Control (AGC) and Receiver Gain Adjust, because these features were designed for test functionality and not for production useGo
-
Added the sentence that starts "For applications in which the TRF7964A may be subjected..." in the second paragraph of Section 6.3, Power SuppliesGo
-
Changed VDD_A to VDD_X in the last sentence that reads "The VDD_X output current should not exceed 20 mA." in the NOTE in Analog Supply Regulator: VDD_AGo
-
Removed the paragraph that started "The RF power amplifier regulator..." from Digital Supply Regulator: VDD_X Go
-
Added the paragraph that starts "As VDD_RF is increased, the system..." in Section 6.3.2, Supply Regulator Settings Go
-
Removed the paragraphs that started "The main receiver also has..." and "By default, the AGC window comparator..." from Section 6.4.2, Receiver Gain and Filter Stages Go
-
Changed Table 6-5 to match Table 6-31Go
-
Updated Section 6.5, Receiver – Digital Section, to clarify and remove duplicate contentGo
-
Updated the description in Section 6.5.1.2, External RSSIGo
-
Removed "Equivalent Series Resistance" from Table 6-8, Minimum Crystal RecommendationsGo
-
Removed mention of 3-wire SPI and replaced "IRQ" with "Slave Select" in the first paragraph of Section 6.10.1, General IntroductionGo
-
Updated the description of FIFO level interrupts in Section 6.10.1.4, FIFO OperationGo
-
Added "but recommended" to "It is optional but recommended to read the FIFO Status register..." in Section 6.10.3, Reception of Air Interface DataGo
-
Changed the title of Section 6.10.4, Data Transmission From MCU to TRF7964AGo
-
Removed the sentence that started "The choice of one of these modes over another..." from Section 6.10.5, Serial Interface Communication (SPI)Go
-
Updated the paragraph that starts "TI recommends resetting the FIFO after receiving data..." in Section 6.10.5.1, Serial Interface Mode With Slave Select (SS)Go
-
Added the NOTE that starts "An additional direct mode..." in Section 6.10.6, Direct ModeGo
-
Added Section 6.11, TRF7964A Initialization Go
-
Changed the application report that is referenced in Section 6.12, Special Direct Mode for Improved MIFARE™ CompatibilityGo
-
Added and updated comments in Table 6-14, Address and Command Word Bit DistributionGo
-
Removed unsupported registers (addresses 0x15 to 0x19) in Table 6-16, Register Values After Sending Software Initialization (0x03)Go
-
Added "This is used by the ISO/IEC 15693 protocol" to Section 6.13.1.8, Transmit Next Time Slot (0x14)Go
-
Corrected description of B1 Irq_col in Table 6-37, IRQ Status Register (0x0C): changed from "(as defined in register 0x01)" to "(as defined in register 0x10)" Go
-
Changed the description of B5:B3 in Table 6-40 from "...Auxiliary RSSI represents the signal level at RX_IN2" to "...Auxiliary RSSI represents the signal level at RX_IN1"Go
-
Updated the description in Section 7.1.2, SchematicGo
-
Section 8.1、「使い始めと次の手順」を追加Go
-
Section 8.2、「デバイスの項目表記」を追加Go
-
Section 8.3、「ツールとソフトウェア」を追加Go
-
Section 8.4、「ドキュメントのサポート」を更新Go