DLPU126 December 2023 DLP470TE , DLP660TE , DLP780TE , DLPC4420
Before programming the DLPC4420AEVM, make sure the DLPC44xx GUI and DMD firmware have both been downloaded to the PC. The DLPC44xx GUI allows for operation of the EVM and the DMD firmware is required according to DMD being utilized. If the DLP660TEEVM is being used with the DLPC4420AEVM, then the DLP660TE firmware is needed. Otherwise, if the DLP470TEEVM is used, then the DLP470TE firmware is needed.
The DMD firmware and DLPC44xx GUI can be found under the Software Development tab on the product pages on TI.com. Please see the product pages for the DLP660TE, DLP470TE, DLP780TE, and DLPC4420.