JAJSG28F august 2018 – august 2020 TPS2120 , TPS2121
PRODUCTION DATA
The load current is monitored at all times. When the load current exceed the current limit trip point ILM programmed by RILM resistor, the device regulates the current within tILM. The following equations can be used to find the RILM value for a desired current limit, where RILM is in kΩ and between 18 kΩ to 100 kΩ.
During current regulation, the output voltage will drop resulting in increased device power dissipation. If the device junction temperature (TJ) reaches the thermal shutdown threshold (TSD) the internal FETs are turned off. After cooling down, the device will automatically restart.