SBAA583 july 2023 PCM1820 , PCM1820-Q1 , PCM1821 , PCM1821-Q1 , PCM1822 , PCM1822-Q1 , PCM3120-Q1 , PCM5120-Q1 , PCM6120-Q1 , TLV320ADC3120 , TLV320ADC5120 , TLV320ADC6120
Features: Good common mode rejection - 80 db
This implementation uses the POM-2730L-HD-R microphone with TLV320ADC6210 ADC.
POM-2730L-HD-R Specifications:
Sensitivity -30db 0db=1V/Pascal with load resistor, output impedance 2.2 kΩ, SNR 74 db SPL of 94 db or 1 Pascal.
TLV320ADCX120 Settings:
The following figures illustrate the circuit for a electret condensor microphone set up to give a differential output.
The output stage of an electret condenser microphone is a FET element. A pull-up to MicBias and pull-down to ground results in the circuit working as a phase splitter. With an incoming sound input, the INxP and INxM pins are moving in phase opposition. When the level of INxP reduces, the level of INxM increases. To achieve the maximum undistorted signal handling, the voltage difference between INxP and INxM must always be greater then zero at the peak of the signal. This keeps the FET element of the microphone working in linear range.
For maximum signal handling the static DC bias across the microphone terminal is kept at VMICBIAS/2.
In this system .
The DC level on the INxP and INxM pins without any audio signal is 2.25 V and 0.75 V respectively. Sounds received by the microphone result in out-of-phase signals on the pins as shown by the figure.
1-VRMS differential signal can be digitized by this circuit.