SBAU382A November 2021 – January 2022 ADS7029-Q1 , ADS7039-Q1 , ADS7040 , ADS7041 , ADS7042 , ADS7043 , ADS7044 , ADS7046 , ADS7047 , ADS7049-Q1 , ADS7052 , ADS7054 , ADS7056 , ADS7057
Download the latest version of the EVM GUI installer from the Order & Start Development section of the ADS7042EVM-PDK, ADS7049-Q1EVM-PDK, or ADS7057EVM-PDK tool folder. Run the GUI installer to install the EVM GUI software on your computer.
As shown in Figure 3-1, accept the license agreements and follow the on-screen instructions to complete the installation.
As part of the ADS704X-5XEVM GUI installation, a prompt with a Device Driver Installation appears on the screen, as shown in Figure 3-2. Click Next to proceed.
The ADS704X-5XEVM requires the LabVIEW™ run-time engine and may prompt for the installation of this software, as shown in Figure 3-3, if not already installed.