SBAU412A November 2022 – May 2024 AFE7900 , AFE7903 , AFE7906 , AFE7920 , AFE7921 , AFE7950
This tutorial guides through the process of using Xilinx Vivado and Vitis development environments to bring up Serial Peripheral Interface (SPI) and non-timing critical General-Purpose Outputs (GPOs) for Texas Instruments AFE79xx EVM along with the companion LMK series clocking chip, thereby enabling an easier integration of the AFE79xx device into a system design. This guide will demonstrate how to use a Xilinx ZCU102 setup as an example.