SBOU298 March 2024 INA4230 , INA4235
To use the EVM with the SCB Controller (sold separately), connect the EVM as shown in Figure 3-1.
If using multiple EVMs (GUI support coming soon), then connect as shown in Figure 3-2. Make sure to use a different address for each device. The GUI only supports one EVM and device type at a time; up to four EVMs total.