SBOU298 March 2024 INA4230 , INA4235
If desired, this EVM and GUI can be used with the PAMB Controller (DC081A) by jumper wiring the pin headers of the PAMB to the EVM. Figure 3-5 shows which pins on the PAMB correspond to the EVM header pins. Note not to add too much resistance in the jumper wire connection setup or the signal can degrade and cause communication errors.
The new GUI and firmware can also be used with the SENS112 and PAMB Controller. If the firmware does not update automatically, then DFU mode can need to be entered manually. See Firmware DebugFirmware Debug.