To set up the GUI the first time:
- Make sure that the previously mentioned driver was
installed successfully to verify the GUI works properly and that the GUI can
update the EVM firmware, if necessary.
- Check to make sure the EVM/SCB Controller unit is
plugged into the PC, then go to the previously provided GUI link.
- Open the GUI Composer application to launch
the GUI from the web browser (see Figure 4-2).
- The GUI link brings up all
versions of the GUI. TI recommends to launch the newest version
available.
- For first-time GUI Composer
setup, follow the prompts to download the TI Cloud Agent and
browser extension (see Figure 4-3). These prompts appears after closing the README.md dialog
box.
- To download the GUI for offline use, click the
icon in the GUI Composer application and
follow the prompts (see Figure 4-2).