SLAAEO8 October 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3519 , MSPM0L1105
RC filters are low-pass filters that can filter out high-frequency noise in the ADC input by selecting an appropriate filter bandwidth. On the one hand, it is hoped that the bandwidth will be as low as possible to cut off high-frequency noise, but on the other hand, excessive bandwidth limitations will prolong the establishment time of the sampling signal and cause input signal distortion. Therefore, it is necessary to design appropriate RC values to filter out high-frequency noise while ensuring timely response to high-frequency signals. Specific reference: Theoretical calculation method of filter RC selection