SLAU367P October 2012 – April 2020 MSP430FR5041 , MSP430FR5043 , MSP430FR50431 , MSP430FR5847 , MSP430FR58471 , MSP430FR5848 , MSP430FR5849 , MSP430FR5857 , MSP430FR5858 , MSP430FR5859 , MSP430FR5867 , MSP430FR58671 , MSP430FR5868 , MSP430FR5869 , MSP430FR5870 , MSP430FR5872 , MSP430FR58721 , MSP430FR5887 , MSP430FR5888 , MSP430FR5889 , MSP430FR58891 , MSP430FR5922 , MSP430FR59221 , MSP430FR5947 , MSP430FR59471 , MSP430FR5948 , MSP430FR5949 , MSP430FR5957 , MSP430FR5958 , MSP430FR5959 , MSP430FR5962 , MSP430FR5964 , MSP430FR5967 , MSP430FR5968 , MSP430FR5969 , MSP430FR5969-SP , MSP430FR59691 , MSP430FR5970 , MSP430FR5972 , MSP430FR59721 , MSP430FR5986 , MSP430FR5987 , MSP430FR5988 , MSP430FR5989 , MSP430FR5989-EP , MSP430FR59891 , MSP430FR5992 , MSP430FR5994 , MSP430FR59941 , MSP430FR6005 , MSP430FR6007 , MSP430FR6035 , MSP430FR6037 , MSP430FR60371 , MSP430FR6041 , MSP430FR6043 , MSP430FR60431 , MSP430FR6045 , MSP430FR6047 , MSP430FR60471 , MSP430FR6820 , MSP430FR6822 , MSP430FR68221 , MSP430FR6870 , MSP430FR6872 , MSP430FR68721 , MSP430FR6877 , MSP430FR6879 , MSP430FR68791 , MSP430FR6887 , MSP430FR6888 , MSP430FR6889 , MSP430FR68891 , MSP430FR6920 , MSP430FR6922 , MSP430FR69221 , MSP430FR6927 , MSP430FR69271 , MSP430FR6928 , MSP430FR6970 , MSP430FR6972 , MSP430FR69721 , MSP430FR6977 , MSP430FR6979 , MSP430FR69791 , MSP430FR6987 , MSP430FR6988 , MSP430FR6989 , MSP430FR69891
SUBX.A | Subtract source address-word from destination address-word | ||
SUBX.[W] | Subtract source word from destination word | ||
SUBX.B | Subtract source byte from destination byte | ||
Syntax | SUBX.A src,dst | ||
SUBX src,dst or SUBX.W src,dst | |||
SUBX.B src,dst | |||
Operation | (.not. src) + 1 + dst → dst or dst – src → dst | ||
Description | The source operand is subtracted from the destination operand. This is done by adding the 1s complement of the source + 1 to the destination. The source operand is not affected. The result is written to the destination operand. Both operands may be located in the full address space. | ||
Status Bits | N: | Set if result is negative (src > dst), reset if positive (src ≤ dst) | |
Z: | Set if result is zero (src = dst), reset otherwise (src ≠ dst) | ||
C: | Set if there is a carry from the MSB, reset otherwise | ||
V: | Set if the subtraction of a negative source operand from a positive destination operand delivers a negative result, or if the subtraction of a positive source operand from a negative destination operand delivers a positive result, reset otherwise (no overflow) | ||
Mode Bits | OSCOFF, CPUOFF, and GIE are not affected. | ||
Example | A 20-bit constant 87654h is subtracted from EDE (LSBs) and EDE+2 (MSBs). |
SUBX.A #87654h,EDE ; Subtract 87654h from EDE+2|EDE
Example | A table word pointed to by R5 (20-bit address) is subtracted from R7. Jump to label TONI if R7 contains zero after the instruction. R5 is auto-incremented by 2. R7.19:16 = 0. |
SUBX.W @R5+,R7 ; Subtract table number from R7. R5 + 2
JZ TONI ; R7 = @R5 (before subtraction)
... ; R7 <> @R5 (before subtraction)
Example | Byte CNT is subtracted from the byte R12 points to in the full address space. Address of CNT is within PC ± 512 K. |
SUBX.B CNT,0(R12) ; Subtract CNT from @R12
Note: Use SUBA for the following 2 cases for better density and execution. |
SUBX.A Rsrc,Rdst
SUBX.A #imm20,Rdst