SLAU776A May 2018 – December 2023 ADC12DL2500 , ADC12DL3200
Make sure that the power connections to the EVMs are the correct polarity. Failure to do so may result in immediate damage.
Make sure that the 12-V power supply is connected to the TSW14DL3200EVM and not the ADC12DLXX00EVM. Providing the ADC12DLXX00EVM with 12-V may result in immediate damage.
Leave the TSW14DL3200EVM power switch in the off position until directed later.