SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
The flash controller provides a program verification mechanism to extend the lifetime of the flash bank. During program operations, the CMDDATAx registers are used by the flash controller as a programming bit mask to indicate which specific bits in the flash word require program pulses. As a result, data which is loaded into the CMDDATAx registers before starting the program operation will be lost from the CMDDATAx registers during and/or upon completion of the program operation. If the same data is to be programmed again, the CMDDATAx registers must be re-loaded by software with the correct data values to be programmed.