SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
Several direct clock connections are made in the device to support specific analog functionality:
Direct Connections to ADCs
In addition to receiving ADCCLK to set the sampling window, the ADC modules also receive the direct output of SYSOSC. The SYSOSC direct output to the ADCs is used by the charge pump logic in the ADC modules. SYSOSC can be configured at any frequency to support this function. The ADC supports requesting SYSOSC automatically before a conversion, so there is not a requirement for application software to ensure that SYSOSC is running before triggering an ADC conversion.