SLAU893B October 2023 – July 2024 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1
The device has five reset levels:
The relationships between reset levels are given in Figure 2-7.
(1) An NRST (low <1 s), software boot reset, or WWDT0 violation triggered BOOTRST runs the boot configuration routine but does not reset the LFCLK, LFCLK_IN, and IOMUX configuration of any IO pins used by LFXT or LFCLK_IN..
(3) If a boot fail occurs during execution of the boot configuration routine, a BOOTRST can be generated by SYSCTL to attempt the boot process again from the BOOTRST level. See Section 2.4.1.8.